Hi all,
I am working in a imx6 solo wandboard, in that i need to integrate the camera ov5640 with mipi interface, for that i want to done the mux pad settings for camera data, clock, reset and pwdn, can any one tell me how to do that, i am new to this camera and linux drivers
Thanks,
dhana
Hi,
I believe John Weber's recent kernel release includes a version of arch/arch/mach-mx6/board-wand.c which sets the pads correctly for mipi input from this camera:
https://groups.google.com/d/topic/wandboard/8T9L1LFL0G0/discussion
The relevant snippets are below:
#ifdef CONFIG_IMX_HAVE_PLATFORM_IMX_MIPI_CSI2
/****************************************************************************
*
* MIPI CSI
*
****************************************************************************/
static void wand_mipi_sensor_io_init(void)
{
struct clk *mipi_csi_mclk;
int rate;
IMX6_SETUP_PAD(GPIO_3__CCM_CLKO2); /* Camera clock */
IMX6_SETUP_PAD(KEY_COL4__GPIO_4_14);/* Camera reset */
IMX6_SETUP_PAD(GPIO_6__GPIO_1_6); /* Camera power down */
pr_debug("%s\n", __func__);
gpio_request(WAND_MIPICSI_RESET, "cam-reset");
gpio_direction_output(WAND_MIPICSI_RESET, 1);
gpio_request(WAND_MIPICSI_PWN, "cam-pwdn");
gpio_direction_output(WAND_MIPICSI_PWN, 1);
/* Master clock for the sensor */
mipi_csi_mclk = clk_get(NULL, "clko2_clk");
if (IS_ERR(mipi_csi_mclk)) {
pr_err("can't get CLKO2 clock.\n");
return;
}
rate = clk_round_rate(mipi_csi_mclk, 24000000);
clk_set_rate(mipi_csi_mclk, rate);
clk_enable(mipi_csi_mclk);
msleep(5);
/* Power up */
gpio_set_value(WAND_MIPICSI_PWN, 0);
msleep(5);
/* Reset on */
gpio_set_value(WAND_MIPICSI_RESET, 0);
msleep(1);
/* Reset off */
gpio_set_value(WAND_MIPICSI_RESET, 1);
msleep(5);
/* power down */
gpio_set_value(WAND_MIPICSI_PWN, 1);
/* For MX6Q:
* GPR1 bit19 and bit20 meaning:
* Bit19: 0 - Enable mipi to IPU1 CSI0
* virtual channel is fixed to 0
* 1 - Enable parallel interface to IPU1 CSI0
* Bit20: 0 - Enable mipi to IPU2 CSI1
* virtual channel is fixed to 3
* 1 - Enable parallel interface to IPU2 CSI1
* IPU1 CSI1 directly connect to mipi csi2,
* virtual channel is fixed to 1
* IPU2 CSI0 directly connect to mipi csi2,
* virtual channel is fixed to 2
*
* For MX6DL:
* GPR13 bit 0-2 IPU_CSI0_MUX
* 000 MIPI_CSI0
* 100 IPU CSI0
*/
if (cpu_is_mx6q())
mxc_iomux_set_gpr_register(1, 19, 1, 0);
else if (cpu_is_mx6dl())
mxc_iomux_set_gpr_register(13, 0, 3, 0);
}
static void wand_mipi_powerdown(int powerdown)
{
pr_debug("%s: powerdown=%d\n", __func__, powerdown);
if (powerdown)
gpio_set_value(WAND_MIPICSI_PWN, 1); /* Power off */
else
gpio_set_value(WAND_MIPICSI_PWN, 0); /* Power on */
msleep(2);
}
/* Platform data for CSI sensor driver, passed to driver
through i2c platform data */
static struct fsl_mxc_camera_platform_data wand_mipi_csi2_data = {
.mclk = 24000000,
.mclk_source = 0,
.csi = 0,
.io_init = wand_mipi_sensor_io_init,
.pwdn = wand_mipi_powerdown,
};
/* TODO - reorg code so that adding i2c board info is done all in one
step at init. This makes adding I2C devices easier */
static struct i2c_board_info wand_mipi_csi_i2c_board_info[] __initdata = {
{
I2C_BOARD_INFO("ov5640_mipi", 0x3C),
.platform_data = (void *)&wand_mipi_csi2_data,
},
{
I2C_BOARD_INFO("ov5647_mipi", 0x36),
.platform_data = (void *)&wand_mipi_csi2_data,
},
};
/* Platform data for MIPI CSI init */
static struct mipi_csi2_platform_data wand_mipi_csi2_platform_data = {
.ipu_id = 0,
.csi_id = 0,
.v_channel = 0,
.lanes = 2,
.dphy_clk = "mipi_pllref_clk",
.pixel_clk = "emi_clk",
};
HTH,
Dave
Hi Dave
Thank you very much.
Best
Andy
发件人: Dave McMordie
发送时间: 2013年8月28日 20:58
收件人: imx6 zeng
主题: Re: - ENABLE MIPI FOR I.MX6 SOLO BOARD
<https://community.freescale.com/> Freescale Community
ENABLE MIPI FOR I.MX6 SOLO BOARD
reply from Dave <https://community.freescale.com/people/davemcmordie?et=watches.email.thread> McMordie in i.MX Community - View <https://community.freescale.com/message/347182?et=watches.email.thread#347182> the full discussion