Hi Artur,
I only find this below, please see "is change this 6 to 7 ?";
The i.MX6 series processors do not support the eMMC 5.0 specification in hardware. Only the backward-compatible eMMC 4.4 use is possible.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
So, how to modify this(use eMMC 5.0 as eMMC 4.4) int BSP version 4.1.15-2.0.1?
The "mmc_read_ext_csd" function is not the same as "https://community.nxp.com/docs/DOC-332187" said.
Thanks,
Cily