Hi team,
I am using the imx8qxp-mek board and using the weston version 10.0.0.4 and wayland of version 1.32 as per mickledore L6.1.36 version.
I am using the below weston configuration
-Dbackend-default=auto \
-Dbackend-rdp=false \
-Dpipewire=false \
-Dremoting=false \
-Dshell-desktop=true \
-Dsystemd=true \
-Dbackend-drm=true \
-Dlauncher-logind=true \
-Ddeprecated-weston-launch=true \
-Drenderer-gl=true
and below weston service file
But when running the weston service I am seeing the below error log msg and weston is not able to run.
Loading module '/usr/lib/aarch64-linux-gnu/libweston-10/gl-renderr
er.so'
[20:24:30.071] EGL client extensions: EGL_EXT_client_extensions
EGL_EXT_platform_base EGL_KHR_platform_wayland
EGL_EXT_platform_wayland EGL_EXT_device_query
EGL_EXT_device_drm EGL_EXT_device_drm_render_node
EGL_KHR_platform_gbm
[20:24:30.072] failed to initialize display
[20:24:30.072] EGL error state: EGL_NOT_INITIALIZED (0x3001)
[20:24:30.072] failed to initialize egl
Could someone please suggest some input on this error
Regards,
Rk
Why do you need modify weston configuration ?
Are you change any other thing in default bsp, like change weston source from mainline?
Hi @Zhiming_Liu , thanks for reply,
What is the default configuration for weston 10.0.0.4 for using weston as backend. ?
I am using those configuration as it required.
Since i cross checked i have all the libs required for gl-render and remaining libs in proper path .
Could you please suggest to have best configuration for weston .
Regards,
Rk
Hi @rakesh3
You can refer the /ect/systemd/system/graphical.target.wants/weston.service and /etc/xdg/weston/weston.ini in BSP.
Hi Team,
Could anyone please suggest on this issue.