E-Ink or E-Paper Displays for i.MX 6ULL evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

E-Ink or E-Paper Displays for i.MX 6ULL evk

ソリューションへジャンプ
2,040件の閲覧回数
fahadusman
Contributor III

Hi, we want to attach an e-ink display with i.MX6ULL evk board, can someone point me to the list of compatible e-ink displays for this device?

Thanks and Regards,

Fahad Usman.

ラベル(1)
0 件の賞賛
1 解決策
1,669件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean mx6ull evk? imx6ull evk board don't have Eink socket

元の投稿で解決策を見る

6 返答(返信)
1,669件の閲覧回数
fahadusman
Contributor III

Yes, I was particularly asking about i.MX 6ULL-evk. This answers my question.

Thanks

0 件の賞賛
1,669件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

The EPDC connector is only for the NXP DC-4 board, whose part number is X-IMXEBOOKDC4

0 件の賞賛
1,669件の閲覧回数
fahadusman
Contributor III

We have an X-IMXEBOOKDC4 display that we have used with i.MX7D in past. But unlike i.MX7d, i.MX6ULL does not have an EPD connector. Please guide me how do we attach the EPD with i.MX6ULL. The part number of i.MX6ULL board we have is MCIMX6ULL-EVK (MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP).

Thanks.

0 件の賞賛
1,669件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it seems this board doesn't support Eink, but mx6ull can support it, you can refer to the mx6ull schmatic to try to change

refer to the mx6ull main page:

Display

  • Parallel LCD Display up to WXGA (1366x768)
  • 8/10/16/24-bit Parallel Camera Sensor Interface
  • Electrophoretic display controller support direct-driver for E-Ink EPD panel, with up to 2048x1536 resolution at 106 Hz
0 件の賞賛
1,669件の閲覧回数
fahadusman
Contributor III

Is there any i.MX6ULL variant that would accept e-paper display out of the box?

0 件の賞賛
1,670件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean mx6ull evk? imx6ull evk board don't have Eink socket