Hi, trying to integrate a fullHD panel on our imx6Q custom board. We are using dual channel lvds in split mode. The display is an innolux G156HCE_L01. The colors are all wrong, as seen in the attached pic, background should be black but displayed blue, the three stripes should be Red, Green and Blue.
This is our current dts config:
/*Dual channel lvds fullHD screen*/
&mxcfb1
{
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB24";
mode_str="LDB-1080P60";
default_bpp = <32>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
&ldb
{
status = "okay";
split-mode;
lvds-channel@0
{
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
display-timings
{
native-mode = <&timing0>;
timing0: hsd100pxn1 {
clock-frequency = <140000000>;
hactive = <1920>;
vactive = <1080>;
hback-porch = <100>;
hfront-porch = <40>;
vback-porch = <30>;
vfront-porch = <3>;
hsync-len = <10>;
vsync-len = <2>;
};
};
};
lvds-channel@1
{
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
primary;
status = "okay";
display-timings
{
native-mode = <&timing1>;
timing1: hsd100pxn1
{
clock-frequency = <140000000>;
hactive = <1920>;
vactive = <1080>;
hback-porch = <100>;
hfront-porch = <40>;
vback-porch = <30>;
vfront-porch = <3>;
hsync-len = <10>;
vsync-len = <2>;
};
};
};
};
Any hint would be appreciated
Hi Andrea
one can check similar case on
linux-imx6/imx6qdl-eo.dtsi at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------