Drive state unknown during reset in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drive state unknown during reset in i.MX6DQ.

ソリューションへジャンプ
869件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to "Table 101. Signals with Differing Before Reset and After Reset States" in IMX6DQAEC(Rev.3)

GPIO_17, GPIO_19 and, KEY_COL0 Values are "Drive state unknown ( x )".

Q1.

What is the meaning of "Drive state unknown ( x )"?

Q2.

My customer would like to fix the Hi or Lo only during reset.

Do you have any solution ? (Add external schematic? or Set by software?)

Best Regards,

Keita

ラベル(3)
0 件の賞賛
1 解決策
778件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

meaning of "Drive state unknown is that value

may be random state (it is not initialized internally by processor).

Seems as external schematic is solution, since

it can not be set by software, because software can be run

only after processor reset. Table 100 shows state immediately

after reset, Table 101 - before reset.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
779件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

meaning of "Drive state unknown is that value

may be random state (it is not initialized internally by processor).

Seems as external schematic is solution, since

it can not be set by software, because software can be run

only after processor reset. Table 100 shows state immediately

after reset, Table 101 - before reset.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
778件の閲覧回数
keitanagashima
Senior Contributor I

Hi Igor,

My customer tried to pull-down by 2.2k ohm for GPIO_19.

But, it remained about 2V.

So, could you tell me the drive ability in case of the Before Reset State condition?

Best Regards,

Keita

0 件の賞賛
778件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

suggest not to use pull resistors,

try tri-state circuit, so i.MX6 pad

was fully isolated from external chip.

~igor

778件の閲覧回数
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your special support.

OK. I got it.

Best Regards,

Keita

0 件の賞賛