Does not boot of RAW NAND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does not boot of RAW NAND

Jump to solution
1,216 Views
takashitakahash
Contributor III

In the description of the i.MX6DQ RM of sect  8.5.2.3 Firmware Configuration Block,

If does not Boot from RAW NAND flash, may not be held in the NAND flash in this format?

Labels (2)
0 Kudos
Reply
1 Solution
1,071 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tahashi

right, if boot from NAND flash is not used

this format (FCB) can be omited.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,072 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tahashi

right, if boot from NAND flash is not used

this format (FCB) can be omited.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply