Does mx8 support 8 Lane Mipi output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does mx8 support 8 Lane Mipi output

999 次查看
ysgou
Contributor I

Hello everyone,

I have a case about video display (mipi output). The customer (oled manufacturer ) requirement  is:

cpu (mipi output) ->  oled panel( 4K resolution)

I want to use i.MX8QUADMAX cpu to design  this project. my question is:

Does i.MX8quadmax support 8 lane mipi output (4k resolution)?

the IMX8QMAEC.pdf document said: 

"This processor supports a single 4K display (with multiple display output options, including MIPI-DSI, HDMI, eDP/DP, and LVDS), or multiple smaller displays."

"Supports single UltraHD 4Kp60 display or up to 4 independent FullHD 1080p60 displays"

"Display IO :  2× MIPI-DSI with 4 lanes each"

Can I combine 2 x mipi-dsi  channels to  a 8 lane mipi output (4k resolution) ?

0 项奖励
回复
2 回复数

959 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello William,

You can have 2 MIPI with 4 lanes each one, so you can have 8 lane for both at 4K.

Regards

0 项奖励
回复

564 次查看
WayneLiao
Contributor I

Hi,

Not understand the reply much.

By the reply, can we use a DSI to HDMI transmitter which use DSI 8 lanes combined as input for the 4K 30Hz or 4K  60Hz HDMI output? yes or no?

And, If just use one port (4 lanes DSI), what's the max resolution can it support?

Thanks.

Wayne

0 项奖励
回复