Does imx6ul linux use OCRAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does imx6ul linux use OCRAM?

1,202件の閲覧回数
charlieschultz
Contributor II

The imx6ul RM says it uses some OCRAM during boot, but after that it is free. Does imx6ul linux use OCRAM? In looking at pm-imx6.c, it is not clear to me with respect to the ul version of the imx6.

ラベル(2)
0 件の賞賛
返信
1 返信

1,037件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Charlie

yes uses (seems one can use linker map for that), for example

low power driver, described in attached Linux Manual Chapter 21
Low-level Power Management (PM) Driver.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信