Does imx-android-l5.1.1_2.1.0-ga support DRM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does imx-android-l5.1.1_2.1.0-ga support DRM?

1,266 Views
calvinyu
Contributor II

Hi

We have a project which uses iMx6 Quad and Android 5.1.

The BSP version is imx-android-l5.1.1_2.1.0-ga.

There are 2 questions.

1. Does the imx-android-l5.1.1_2.1.0-ga BSP support DRM feature?

2. How to write the DRM key to the device ?The DRM key is from google.

B.R

Calvin

0 Kudos
3 Replies

812 Views
pratik0403
Contributor I

Hi,

 

I have couple of questions with the same Widevine compliance on Android.

1. Is "Widevine level 1 compliance for DRM" implemented/available for IMX6 on Android platform? or Do we need to purchase separately?

2. If it is already implemented, then where we can find it's relevant document?

 

Thanks & Regards,

Pratik

0 Kudos

812 Views
igorpadykov
NXP Employee
NXP Employee

Hi Calvin

it is supported as separate patch (not included in default

Android release), note customer needs license with google,

please contact local marketing for that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

812 Views
calvinyu
Contributor II

Hi igor

Thank you for your information.

0 Kudos