Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

1,476 Views
charleshuang
Senior Contributor II

Does i.MX6 support HW acceleration for HTML5 in Chromium on Yocto or LTIB?

If yes, can you tell me how to enable this function?

Thank you.

Best Regards,

Alex Cheng

Labels (5)
0 Kudos
Reply
1 Reply

809 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

chromium-imx recipes support hardware acceleration, refer to attached

Yocto Guide sect.5.6.6 Chromium Browser on X11, XWayland and Wayland

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply