Hi,
I am using i.MX 8M Mini with a v4.19 kernel from NXP/Codeaurora (imx_4.19.35_1.1.0). It's a pretty old release (v4.19.35) from v4.19 stable tree with a lot of unfixed bugs. The current v4.19 kernel is v4.19.130, so almost 100 stable releases further.
These stable releases come with a lot less and more important bug fixes (including security fixes).
The question: Do you plan to provide BSP v4.19 kernel updated to latest stable v4.19 (e.g. v4.19.130) or you expect every customer should perform such important maintenance by himself?
Best regards,
Krzysztof
Hello,
The latest BSP update is the L5.4.3 and you can download from the code aurora as well. there is no any update from the L4.19.35.
Regards