Do you have i.MX6D VDDARM23_IN and VDDARM23_CAP leakage data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you have i.MX6D VDDARM23_IN and VDDARM23_CAP leakage data?

ソリューションへジャンプ
839件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Could you let me know how much leakage from VDDARM23_IN to GND, and from VDDARM23_CAP to GND for i.MX6D design?

Actually, a end user will use the attached design instead of the all-in-one circuit in Figure 1 of AN4397.

Then, they want to estimate the leakage.

Best Regards,

Satoshi Shimoda

ラベル(1)
0 件の賞賛
返信
1 解決策
666件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

In general this leakage current for both signals has the same nature as

leakage for example in DSM mode, that is about 0.1mA.

Please check Table 2 application Note AN4509 (Rev. 0, 10/2012)

"i.MX 6Dual/6Quad Power Consumption Measurement".

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
667件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

In general this leakage current for both signals has the same nature as

leakage for example in DSM mode, that is about 0.1mA.

Please check Table 2 application Note AN4509 (Rev. 0, 10/2012)

"i.MX 6Dual/6Quad Power Consumption Measurement".

0 件の賞賛
返信