Hi,
with a imx53qsb board, DISP0_DCLK,signal present on expansion header at pin 43 doesn't contain pixclk clock signal from display. Other signals like DISP0_VSYNC, DISP0_HSYNC or DISP0_DRDY are however ok.
I plan to connect parallel display port di0 to a lcd and i need DISP_DCLK signal.
Is there any bootargs command or other to activate it ?
Thanks,
Christophe.
已解决! 转到解答。
Hello,Christophe,
The following setting is also OK:
u-boot >setenv bootargs console=ttymxc0 init=/init androidboot.console=ttymxc0 video=mxcdi0fb:RGB24,1280x720M@60 di0_primary hdmi
system will assign memory automatically.
Weidong
Hi,Christophe,
Connect HDMI daughter board and connect HDMI cable to monitor with HDMI, The
Try the following setting for u-boot environment:
u-boot > setenv console=ttymxc0 init=/init androidboot.console=ttymxc0 video=mxcdi0fb:RGB24,1280x720M@60,bpp=32 hdmi di0_primarypmem=64M,64M fbmem=16M gpu_memory=64M
u-boot > save
Regards,
Weidong
Hi Weidong,
It's not really a hdmi problem. But it seems that suppressing ldb extension is enough like below:
set bootargs console=ttymxc0,115200 video=mxcdi0fb:RGB24,720P60 di0_primary.
Netherveless, i take note of your response for further applications.
Rgds,
Christophe
Hi Weidong,
I can see pixclk now. Things are clear on that.
Now, i've tried your bootargs line and imx crashes when booting. Here's the last lines just before the crash:
vmap allocation for size 469766144 failed: use vmalloc=<size> to increase size.
fbcvt: 1280x720@60: CVT Name - .921M9
mxc_ipu mxc_ipu: Channel already disabled 9
mxc_ipu mxc_ipu: Channel already uninitialized 9
IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
The fact is i usually don't reserve memory at boot stage. Is it better ? Can you explain please.
Christophe
Hello,Christophe,
The following setting is also OK:
u-boot >setenv bootargs console=ttymxc0 init=/init androidboot.console=ttymxc0 video=mxcdi0fb:RGB24,1280x720M@60 di0_primary hdmi
system will assign memory automatically.
Weidong