Discharge Circuit for EXT_1V8 on i.MX8QXP MEK can not work well

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Discharge Circuit for EXT_1V8 on i.MX8QXP MEK can not work well

317件の閲覧回数
question2click6
Contributor II

Dear Sir/Madam,

I think the discharge circuit on i.MX8QXP MEK board can not work well if VCC12V0 power down, because:

 if 12V power down will lead VCC_EXT_3V3 at low level, so Q14 will remain at closed state.

pastedImage_1.png

please check on this, thank you!

Wenwen

ラベル(1)
0 件の賞賛
1 返信

271件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wen,

  There are too many caps on the net of VCC_EXT_3V3, the power down sequence of the power rail is later, it can make Q14 open and realize discharged. The circuit is verified on our EVK board.

Hope this can do help for you.

Have a nice day

Rita

0 件の賞賛