Different between kernel 3.0.xx vs 3.10.xx vs 3.14.xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Different between kernel 3.0.xx vs 3.10.xx vs 3.14.xx

1,405件の閲覧回数
zctee
Contributor III

Hi all,

I notice that in the Freescale page for i.mx6, there are 3 version of linux, which are 3.0.101, 3.10.53 and 3.14.28.

i.MX 6 Series Software and Development Tool R|Freescale

May i know what is the different between these 3 version of linux BSP?

Thank you.

Regards,

ZC

ラベル(2)
タグ(2)
0 件の賞賛
3 返答(返信)

699件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZC

difference is decribed in Release Notes document included in

Doc bundle for each package (in particular pay attention to sect.2.x New features)

L3.0.35_4.1.0_LINUX_DOCS

L3.14.28_1.0.0_LINUX_DOCS

L3.10.53_1.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

699件の閲覧回数
zctee
Contributor III

Hi Igor,

It seems like the 3.0.xx is for Debian, while 3.10.xx and 3.14.xx is for yocto. Am i correct to say that?

Thank you.

Regards,

ZC

0 件の賞賛

699件の閲覧回数
zctee
Contributor III

Hi Igor,

Is there any doc package for the 3.0.101? It seems that i only can find latest doc till 3.0.35 in below page:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Regards,

ZC

0 件の賞賛