Details of H.264 encoder support in i.MX8MMini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Details of H.264 encoder support in i.MX8MMini

ソリューションへジャンプ
713件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

I'm investigating a device spec of H.264 encoder in i.MX8MMini.

Could someone teach me following questions ?

Q1.What GOP structure of H.264 Encoder does i.MX8MMini support ?  

Q2.What is the maximum GOP size of the H.264 Encoder (how long can the GOP be extended)?
Q3.What is the CPB (Coded Picture Buffer) size of the H.264 Encoder?
Q4.What is the output format of H.264 Encoder encoded data?
Q5.What is the supported encoding bit depth of H.264 Encoder?

Ko-hey

ラベル(2)
0 件の賞賛
返信
1 解決策
645件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"

Q1.What GOP structure of H.264 Encoder does i.MX8MMini support ? 

[Answer] : gop is used to set interval of I frames

Q2.What is the maximum GOP size of the H.264 Encoder (how long can the GOP be extended)?

[Answer] : [1: 300]

Q3.What is the CPB (Coded Picture Buffer) size of the H.264 Encoder?

[Answer] : it is related with the encoded(compressed) data size, basically, user dont need to handle it

Q4.What is the output format of H.264 Encoder encoded data?

[Answer] : just encoded(compressed) data, not any special format defined

Q5.What is the supported encoding bit depth of H.264 Encoder

[Answer] : only 8 bit

"

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
646件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"

Q1.What GOP structure of H.264 Encoder does i.MX8MMini support ? 

[Answer] : gop is used to set interval of I frames

Q2.What is the maximum GOP size of the H.264 Encoder (how long can the GOP be extended)?

[Answer] : [1: 300]

Q3.What is the CPB (Coded Picture Buffer) size of the H.264 Encoder?

[Answer] : it is related with the encoded(compressed) data size, basically, user dont need to handle it

Q4.What is the output format of H.264 Encoder encoded data?

[Answer] : just encoded(compressed) data, not any special format defined

Q5.What is the supported encoding bit depth of H.264 Encoder

[Answer] : only 8 bit

"

Regards,

Yuri.

0 件の賞賛
返信