Demo for MCIMX6Q-SDB and MCIMX-LVDS1 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Demo for MCIMX6Q-SDB and MCIMX-LVDS1 ?

774 次查看
tj5
Contributor I

I have MCIMX6Q-SDB board and MCIMX-LVDS1 display. I want to run Linux demo to test it.

On website I see many demo packages for i.MX 6Quad, which will be most suitable for my hardware ?

 

 

I'm testing

Source Code Download Steps Documentation and Demo Images (REV L3.10.17_1.0.0)

in log I see

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

and my LCD is black

Original Attachment has been moved to: log.txt.zip

标签 (2)
0 项奖励
2 回复数

546 次查看
art
NXP Employee
NXP Employee

Have you connected your LVDS panel to the correct LVDS port? Please check.

Also, refer to the "video" section on the Page 10 of the attached document for the information on how to set up various display ports including LVDS in the kernel command line.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

546 次查看
tj5
Contributor I

Thank you for reply, now my LCD is working correctly

0 项奖励