Hello.
Trying to debug U-boot on IMX6ULL using this manual.
So I am able to compile U-boot sources using Eclipse and get binary U-boot file.
Enabled debugging options in .config file:
CONFIG_CC_OPTIMIZE_FOR_SIZE=n
CONFIG_TOOLS_DEBUG=y
Here debugger configuration:
Get following logs on starting debugger server:
SEGGER J-Link GDB Server V7.54a Command Line Version
JLinkARM.dll V7.54a (DLL compiled Sep 7 2021 14:25:38)
Command line: -if jtag -device MCIMX6Y2 -endian little -speed auto -port 2331 -swoport 2332 -telnetport 2333 -noir -localhostonly 0 -scriptfile ddr_init.jlinkscript
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: off
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: ddr_init.jlinkscript
J-Link settings file: none
------Target related settings------
Target device: MCIMX6Y2
Target interface: JTAG
Target interface speed: auto
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
Hardware: V8.00
Feature(s): RDI,FlashDL,FlashBP,JFlash,GDB
Checking target voltage...
Target voltage: 3.26 V
Listening on TCP/IP port 2331
Connecting to target...
J-Link found 3 JTAG devices, Total IRLen = 13
JTAG ID: 0x5BA00477 (Cortex-A7)
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x87890988 (Data = 0x00000000)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 2 bytes @ address 0x8785F178 (Data = 0xFFFE)
Read 2 bytes @ address 0x8785F176 (Data = 0xEBFE)
Read 2 bytes @ address 0x8785F174 (Data = 0xD7AE)
Read 2 bytes @ address 0x8785F178 (Data = 0xFFFE)
Read 2 bytes @ address 0x8785F176 (Data = 0xEBFE)
Read 2 bytes @ address 0x8785F174 (Data = 0xD7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F174 (Data = 0xEBFED7AE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Read 4 bytes @ address 0x8785F178 (Data = 0xEAFFFFFE)
Received monitor command: speed 1000
Target interface speed set to 1000 kHz
Received monitor command: clrbp
Received monitor command: reset
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x8785F178)
Received monitor command: regs
PC = 8785F178, CPSR = 600001D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 8785F180, R1 = 8786F6B8, R2 = 00000000, R3 = 0091F78D
R4 = 00000005, R5 = 87800320, R6 = 00000001, R7 = 8FF8D5BA
USR: R8 =8FF9CC8C, R9 =0091FA00, R10=8FF8D5BA, R11 =00000001, R12 =00000031
R13=80DB8C6B, R14=9E4F4394
FIQ: R8 =B6472704, R9 =846B1BF6, R10=DD3BACFE, R11 =EFF1EB7F, R12 =6E6C9283
R13=DC9247E9, R14=1F5A8FEF, SPSR=5A000312
SVC: R13=0091F9F0, R14=8785F178, SPSR=000001D3
ABT: R13=CDF44348, R14=6CA56019, SPSR=10038120
IRQ: R13=E966343D, R14=2AC8E2B6, SPSR=38026A20
UND: R13=7FC7CC2D, R14=11E13C9D, SPSR=20066601
Reading all registers
Received monitor command: speed auto
Select auto target interface speed (1000 kHz)
Received monitor command: flash breakpoints 1
Flash breakpoints enabled
Received monitor command: semihosting enable
Semi-hosting enabled (SVC Addr = 0x08)
Received monitor command: semihosting IOClient 2
Semihosting I/O set to GDB Client
Read 4 bytes @ address 0x87890988 (Data = 0x00000000)
Downloading 16272 bytes @ address 0x87800000
Downloading 16304 bytes @ address 0x87803F90
Downloading 16304 bytes @ address 0x87807F40
Downloading 16272 bytes @ address 0x8780BEF0
Downloading 16304 bytes @ address 0x8780FE80
Downloading 16272 bytes @ address 0x87813E30
Downloading 16288 bytes @ address 0x87817DC0
Downloading 16240 bytes @ address 0x8781BD60
Downloading 16272 bytes @ address 0x8781FCD0
Downloading 16272 bytes @ address 0x87823C60
Downloading 16256 bytes @ address 0x87827BF0
Downloading 16288 bytes @ address 0x8782BB70
Downloading 16272 bytes @ address 0x8782FB10
Downloading 16272 bytes @ address 0x87833AA0
Downloading 16256 bytes @ address 0x87837A30
Downloading 16256 bytes @ address 0x8783B9B0
Downloading 16256 bytes @ address 0x8783F930
Downloading 16304 bytes @ address 0x878438B0
Downloading 16288 bytes @ address 0x87847860
Downloading 16272 bytes @ address 0x8784B800
Downloading 16256 bytes @ address 0x8784F790
Downloading 16288 bytes @ address 0x87853710
Downloading 16160 bytes @ address 0x878576B0
Downloading 16192 bytes @ address 0x8785B5D0
Downloading 16272 bytes @ address 0x8785F510
Downloading 16272 bytes @ address 0x878634A0
Downloading 40 bytes @ address 0x87867430
Downloading 16120 bytes @ address 0x87867458
Downloading 16224 bytes @ address 0x8786B350
Downloading 16192 bytes @ address 0x8786F2B0
Downloading 16336 bytes @ address 0x878731F0
Downloading 16336 bytes @ address 0x878771C0
Downloading 1294 bytes @ address 0x8787B190
Downloading 24 bytes @ address 0x8787B6A0
Downloading 16328 bytes @ address 0x8787B6B8
Downloading 11484 bytes @ address 0x8787F680
Downloading 12 bytes @ address 0x8788235C
Downloading 4616 bytes @ address 0x87882368
Downloading 256 bytes @ address 0x87883570
Downloading 144 bytes @ address 0x87883670
Downloading 16256 bytes @ address 0x87883700
Downloading 16304 bytes @ address 0x87887680
Downloading 16304 bytes @ address 0x8788B630
Downloading 4928 bytes @ address 0x8788F5E0
Downloading 48 bytes @ address 0x87890920
Downloading 1 bytes @ address 0x87890950
Downloading 144 bytes @ address 0x87890954
Downloading 24 bytes @ address 0x878909E4
Writing register (PC = 0x87800000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x8781503C (Data = 0xE52DE004)
Reading 64 bytes @ address 0x87817CC0
Read 4 bytes @ address 0x87817CD8 (Data = 0x8786811C)
Read 4 bytes @ address 0x87817CC8 (Data = 0xE59F0008)
Reading 64 bytes @ address 0x87818080
Read 4 bytes @ address 0x8781809C (Data = 0xE59F0004)
Reading 64 bytes @ address 0x87817E80
Read 4 bytes @ address 0x87817EA4 (Data = 0xEBFFF464)
Read 4 bytes @ address 0x87817EA0 (Data = 0xE92D4010)
Received monitor command: regs
PC = 87800000, CPSR = 600001D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 8785F180, R1 = 8786F6B8, R2 = 00000000, R3 = 0091F78D
R4 = 00000005, R5 = 87800320, R6 = 00000001, R7 = 8FF8D5BA
USR: R8 =8FF9CC8C, R9 =0091FA00, R10=8FF8D5BA, R11 =00000001, R12 =00000031
R13=80DB8C6B, R14=9E4F4394
FIQ: R8 =B6472704, R9 =846B1BF6, R10=DD3BACFE, R11 =EFF1EB7F, R12 =6E6C9283
R13=DC9247E9, R14=1F5A8FEF, SPSR=5A000312
SVC: R13=0091F9F0, R14=8785F178, SPSR=000001D3
ABT: R13=CDF44348, R14=6CA56019, SPSR=10038120
IRQ: R13=E966343D, R14=2AC8E2B6, SPSR=38026A20
UND: R13=7FC7CC2D, R14=11E13C9D, SPSR=20066601
Reading all registers
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 2 bytes @ address 0x87800000 (Data = 0x00B8)
Read 2 bytes @ address 0x877FFFFE (Data = 0x0000)
Read 2 bytes @ address 0x877FFFFC (Data = 0x0000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x877FFFFC (Data = 0x00000000)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Read 4 bytes @ address 0x87800000 (Data = 0xEA0000B8)
Everything looks fine but unfortunately get following error message at debugging window:
Another one thing confusing me is that u-boot console still accessible to enter commands and no reboot messages in console during startng debugging session.
Any hints what did I miss?
Hi Almaz
may be useful below links
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Bring-up-i-MX6-via-JTAG/ta-p/1124954
https://forum.segger.com/index.php/Thread/5165-SOLVED-iMX6UL-DDR-initialization-for-u-boot/
Best regards
igor
Thank you very much for links, Igor!
Checked them carefully. But still can't debug properly.
As there are troubles with Eclipse I decided to try from scratch, e.g. tried to debug from command line.
Here what I did.
Started JLinkGDBServer:
$ JLinkGDBServer -device MCIMX6Y2 -if JTAG -speed 1000
with following logs:
SEGGER J-Link GDB Server V7.54a Command Line Version
JLinkARM.dll V7.54a (DLL compiled Sep 7 2021 14:25:38)
Command line: -device MCIMX6Y2 -if JTAG -speed 1000
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: off
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: MCIMX6Y2
Target interface: JTAG
Target interface speed: 1000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
Hardware: V8.00
Feature(s): RDI,FlashDL,FlashBP,JFlash,GDB
Checking target voltage...
Target voltage: 3.26 V
Listening on TCP/IP port 2331
Connecting to target...
J-Link found 3 JTAG devices, Total IRLen = 13
JTAG ID: 0x5BA00477 (Cortex-A7)
Connected to target
Waiting for GDB connection...
then I created gdb init script based on lauterbach's dcd files and script provided there:
# Initializing target
target remote localhost:2331
monitor reset
monitor halt
monitor sleep 200
# Disable Watchdog
monitor memU32 0x020bc000=0x30
# Enable all clocks
monitor memU32 0x020c4068=0xffffffff
monitor memU32 0x020c406c=0xffffffff
monitor memU32 0x020c4070=0xffffffff
monitor memU32 0x020c4074=0xffffffff
monitor memU32 0x020c4078=0xffffffff
monitor memU32 0x020c407c=0xffffffff
monitor memU32 0x020c4080=0xffffffff
monitor memU32 0x020E04B4=0x000C0000
monitor memU32 0x020E04AC=0x00000000
monitor memU32 0x020E027C=0x00000030
monitor memU32 0x020E0250=0x00000030
monitor memU32 0x020E024C=0x00000030
monitor memU32 0x020E0490=0x00000030
monitor memU32 0x020E0288=0x000C0030
monitor memU32 0x020E0270=0x00000000
monitor memU32 0x020E0260=0x00000030
monitor memU32 0x020E0264=0x00000030
monitor memU32 0x020E04A0=0x00000030
monitor memU32 0x020E0494=0x00020000
monitor memU32 0x020E0280=0x00000030
monitor memU32 0x020E0284=0x00000030
monitor memU32 0x020E04B0=0x00020000
monitor memU32 0x020E0498=0x00000030
monitor memU32 0x020E04A4=0x00000030
monitor memU32 0x020E0244=0x00000030
monitor memU32 0x020E0248=0x00000030
monitor memU32 0x021B001C=0x00008000
monitor memU32 0x021B0800=0xA1390003
monitor memU32 0x021B080C=0x00000004
monitor memU32 0x021B083C=0x41640158
monitor memU32 0x021B0848=0x40403237
monitor memU32 0x021B0850=0x40403C33
monitor memU32 0x021B081C=0x33333333
monitor memU32 0x021B0820=0x33333333
monitor memU32 0x021B082C=0xf3333333
monitor memU32 0x021B0830=0xf3333333
monitor memU32 0x021B08C0=0x00944009
monitor memU32 0x021B08b8=0x00000800
monitor memU32 0x021B0004=0x0002002D
monitor memU32 0x021B0008=0x1B333030
monitor memU32 0x021B000C=0x676B52F3
monitor memU32 0x021B0010=0xB66D0B63
monitor memU32 0x021B0014=0x01FF00DB
monitor memU32 0x021B0018=0x00201740
monitor memU32 0x021B001C=0x00008000
monitor memU32 0x021B002C=0x000026D2
monitor memU32 0x021B0030=0x006B1023
monitor memU32 0x021B0040=0x0000004F
monitor memU32 0x021B0000=0x84180000
monitor memU32 0x021B0890=0x00400000
monitor memU32 0x021B001C=0x02008032
monitor memU32 0x021B001C=0x00008033
monitor memU32 0x021B001C=0x00048031
monitor memU32 0x021B001C=0x15208030
monitor memU32 0x021B001C=0x04008040
monitor memU32 0x021B0020=0x00000800
monitor memU32 0x021B0818=0x00000227
monitor memU32 0x021B0004=0x0002552D
monitor memU32 0x021B0404=0x00011006
monitor memU32 0x021B001C=0x00000000
monitor reg cpsr = 0xD3
monitor reg sp = 0x0093FF20
monitor reg pc = 0x87800000
here is command I start gdb:
$ gdb-multiarch u-boot --nx -ix lauterbach
and it outputs:
0x8ff62d00 in ?? ()
Resetting target
Sleep 200ms
Writing 0x00000030 @ address 0x020BC000
Writing 0xFFFFFFFF @ address 0x020C4068
Writing 0xFFFFFFFF @ address 0x020C406C
Writing 0xFFFFFFFF @ address 0x020C4070
Writing 0xFFFFFFFF @ address 0x020C4074
Writing 0xFFFFFFFF @ address 0x020C4078
Writing 0xFFFFFFFF @ address 0x020C407C
Writing 0xFFFFFFFF @ address 0x020C4080
Writing 0x000C0000 @ address 0x020E04B4
Writing 0x00000000 @ address 0x020E04AC
Writing 0x00000030 @ address 0x020E027C
Writing 0x00000030 @ address 0x020E0250
Writing 0x00000030 @ address 0x020E024C
Writing 0x00000030 @ address 0x020E0490
Writing 0x000C0030 @ address 0x020E0288
Writing 0x00000000 @ address 0x020E0270
Writing 0x00000030 @ address 0x020E0260
Writing 0x00000030 @ address 0x020E0264
Writing 0x00000030 @ address 0x020E04A0
Writing 0x00020000 @ address 0x020E0494
Writing 0x00000030 @ address 0x020E0280
Writing 0x00000030 @ address 0x020E0284
Writing 0x00020000 @ address 0x020E04B0
Writing 0x00000030 @ address 0x020E0498
Writing 0x00000030 @ address 0x020E04A4
Writing 0x00000030 @ address 0x020E0244
Writing 0x00000030 @ address 0x020E0248
Writing 0x00008000 @ address 0x021B001C
Writing 0xA1390003 @ address 0x021B0800
Writing 0x00000004 @ address 0x021B080C
Writing 0x41640158 @ address 0x021B083C
Writing 0x40403237 @ address 0x021B0848
Writing 0x40403C33 @ address 0x021B0850
Writing 0x33333333 @ address 0x021B081C
Writing 0x33333333 @ address 0x021B0820
Writing 0xF3333333 @ address 0x021B082C
Writing 0xF3333333 @ address 0x021B0830
Writing 0x00944009 @ address 0x021B08C0
Writing 0x00000800 @ address 0x021B08B8
Writing 0x0002002D @ address 0x021B0004
Writing 0x1B333030 @ address 0x021B0008
Writing 0x676B52F3 @ address 0x021B000C
Writing 0xB66D0B63 @ address 0x021B0010
Writing 0x01FF00DB @ address 0x021B0014
Writing 0x00201740 @ address 0x021B0018
Writing 0x00008000 @ address 0x021B001C
Writing 0x000026D2 @ address 0x021B002C
Writing 0x006B1023 @ address 0x021B0030
Writing 0x0000004F @ address 0x021B0040
Writing 0x84180000 @ address 0x021B0000
Writing 0x00400000 @ address 0x021B0890
Writing 0x02008032 @ address 0x021B001C
Writing 0x00008033 @ address 0x021B001C
Writing 0x00048031 @ address 0x021B001C
Writing 0x15208030 @ address 0x021B001C
Writing 0x04008040 @ address 0x021B001C
Writing 0x00000800 @ address 0x021B0020
Writing 0x00000227 @ address 0x021B0818
Writing 0x0002552D @ address 0x021B0004
Writing 0x00011006 @ address 0x021B0404
Writing 0x00000000 @ address 0x021B001C
Writing register (F0 = 0x000000D3)
Writing register (SP = 0x0093FF20)
Writing register (PC = 0x87800000)
Reading symbols from u-boot...
then I:
(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 718 KB/sec, 12341 bytes/write.
and:
(gdb) s
Cannot access memory at address 0x87800000
while gdb server:
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFE
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFE
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x877FFFFC
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000
WARNING: Failed to read memory @ address 0x87800000
Unable to access DDR memory.
After that I rebooted device, restarted GDB server using same command an started gdb in following way:
$ gdb-multiarch u-boot --nx
and typed:
(gdb) target remote localhost:2331
Remote debugging using localhost:2331
0x8ff62d00 in ?? ()
(gdb) monitor reset
Resetting target
(gdb) monitor halt
(gdb) monitor sleep
Expected an decimal digit (0-9)
(gdb) monitor sleep 200
Sleep 200ms
(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.
Then:
(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40 b save_boot_params
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116 b save_boot_params_ret @ back to my caller
(gdb) s
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:56
56 mrs r0, cpsr
(gdb) s
57 and r1, r0, #0x1f @ mask mode bits
(gdb) s
58 teq r1, #0x1a @ test for HYP mode
looks like I started to debug source code technically, but then:
Breakpoint 1 at 0x878020f4: file arch/arm/imx-common/cpu.c, line 184.
(gdb) c
Continuing.
s
c
^C
Program received signal SIGTRAP, Trace/breakpoint trap.
0x8785f178 in bootstage_error (id=BOOTSTAGE_ID_NEED_RESET) at include/bootstage.h:387
387 show_boot_progress(-id);
E.g. it stuck somewhere until I pressed CTRL-C.
Repeated GdbServer and gdb restarting and passed same steps and it exited at another source code line.
So I repeated everything again and went step by step:
Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.
(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40 b save_boot_params
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116 b save_boot_params_ret @ back to my caller
(gdb)
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:56
56 mrs r0, cpsr
(gdb)
57 and r1, r0, #0x1f @ mask mode bits
(gdb)
58 teq r1, #0x1a @ test for HYP mode
(gdb)
59 bicne r0, r0, #0x1f @ clear all mode bits
(gdb)
60 orrne r0, r0, #0x13 @ set SVC mode
(gdb) s
61 orr r0, r0, #0xc0 @ disable FIQ and IRQ
(gdb) s
62 msr cpsr,r0
(gdb) s
71 mrc p15, 0, r0, c1, c0, 0 @ Read CP15 SCTLR Register
(gdb) s
72 bic r0, #CR_V @ V = 0
(gdb) s
73 mcr p15, 0, r0, c1, c0, 0 @ Write CP15 SCTLR Register
(gdb) s
76 ldr r0, =_start
(gdb) s
77 mcr p15, 0, r0, c12, c0, 0 @Set VBAR
(gdb) s
82 bl cpu_init_cp15
(gdb) s
cpu_init_cp15 () at arch/arm/cpu/armv7/start.S:139
139 mov r0, #0 @ set up for MCR
(gdb) s
140 mcr p15, 0, r0, c8, c7, 0 @ invalidate TLBs
(gdb) s
141 mcr p15, 0, r0, c7, c5, 0 @ invalidate icache
(gdb) s
142 mcr p15, 0, r0, c7, c5, 6 @ invalidate BP array
(gdb) s
143 mcr p15, 0, r0, c7, c10, 4 @ DSB
(gdb) s
144 mcr p15, 0, r0, c7, c5, 4 @ ISB
(gdb) s
149 mrc p15, 0, r0, c1, c0, 0
(gdb) s
150 bic r0, r0, #0x00002000 @ clear bits 13 (--V-)
(gdb) s
151 bic r0, r0, #0x00000007 @ clear bits 2:0 (-CAM)
(gdb) s
152 orr r0, r0, #0x00000002 @ set bit 1 (--A-) Align
(gdb) s
153 orr r0, r0, #0x00000800 @ set bit 11 (Z---) BTB
(gdb) s
157 orr r0, r0, #0x00001000 @ set bit 12 (I) I-cache
(gdb) s
159 mcr p15, 0, r0, c1, c0, 0
(gdb) s
190 mov r5, lr @ Store my Caller
(gdb) s
191 mrc p15, 0, r1, c0, c0, 0 @ r1 has Read Main ID Register (MIDR)
(gdb) s
192 mov r3, r1, lsr #20 @ get variant field
(gdb) s
193 and r3, r3, #0xf @ r3 has CPU variant
(gdb) s
194 and r4, r1, #0xf @ r4 has CPU revision
(gdb) s
195 mov r2, r3, lsl #4 @ shift variant field for combined value
(gdb) s
196 orr r2, r4, r2 @ r2 has combined CPU variant + revision
(gdb) s
298 mov pc, r5 @ back to my caller
(gdb) s
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:84
84 bl cpu_init_crit
(gdb) s
cpu_init_crit () at arch/arm/cpu/armv7/start.S:318
318 b lowlevel_init @ go setup pll,mux,memory
(gdb) s
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:32
32 ldr sp, =CONFIG_SYS_INIT_SP_ADDR
(gdb) s
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:34
34 bic sp, sp, #7 /* 8-byte alignment for ABI compliance */
(gdb) s
45 sub sp, sp, #GD_SIZE
(gdb) s
46 bic sp, sp, #7
(gdb) s
47 mov r9, sp
(gdb) s
53 push {ip, lr}
(gdb) s
68 bl s_init
(gdb)
s_init () at arch/arm/cpu/armv7/mx6/soc.c:588
588 if (is_mx6sx() || is_mx6ul() || is_mx6ull())
(gdb) s
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69 u32 reg = readl(&anatop->digprog_sololite);
(gdb) s
70 u32 type = ((reg >> 16) & 0xff);
(gdb)
73 if (type != MXC_CPU_MX6SL) {
(gdb)
74 reg = readl(&anatop->digprog);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
77 type = ((reg >> 16) & 0xff);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
78 if (type == MXC_CPU_MX6DL) {
(gdb)
83 if (type == MXC_CPU_MX6Q) {
(gdb)
89 major = ((reg >> & 0xff);
(gdb)
90 if ((major >= 1) &&
(gdb)
67 {
(gdb)
98 return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb)
99 }
(gdb)
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69 u32 reg = readl(&anatop->digprog_sololite);
(gdb)
70 u32 type = ((reg >> 16) & 0xff);
(gdb)
73 if (type != MXC_CPU_MX6SL) {
(gdb)
74 reg = readl(&anatop->digprog);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
77 type = ((reg >> 16) & 0xff);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
78 if (type == MXC_CPU_MX6DL) {
(gdb)
83 if (type == MXC_CPU_MX6Q) {
(gdb)
89 major = ((reg >> & 0xff);
(gdb)
90 if ((major >= 1) &&
(gdb)
67 {
(gdb)
98 return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb)
99 }
(gdb)
get_cpu_rev () at arch/arm/cpu/armv7/mx6/soc.c:69
69 u32 reg = readl(&anatop->digprog_sololite);
(gdb)
70 u32 type = ((reg >> 16) & 0xff);
(gdb)
73 if (type != MXC_CPU_MX6SL) {
(gdb)
74 reg = readl(&anatop->digprog);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
77 type = ((reg >> 16) & 0xff);
(gdb)
76 cfg = readl(&scu->config) & 3;
(gdb)
78 if (type == MXC_CPU_MX6DL) {
(gdb)
83 if (type == MXC_CPU_MX6Q) {
(gdb)
89 major = ((reg >> & 0xff);
(gdb)
90 if ((major >= 1) &&
(gdb)
67 {
(gdb)
98 return (type << 12) | (reg + (0x10 * (major + 1)));
(gdb)
99 }
(gdb)
lowlevel_init () at arch/arm/cpu/armv7/lowlevel_init.S:69
69 pop {ip, pc}
(gdb)
save_boot_params_ret () at arch/arm/cpu/armv7/start.S:88
88 bl _main
(gdb)
_main () at arch/arm/lib/crt0.S:76
76 ldr r0, =(CONFIG_SYS_INIT_SP_ADDR)
(gdb) s
78 bic r0, r0, #7 /* 8-byte alignment for ABI compliance */
(gdb)
79 mov sp, r0
(gdb)
_main () at arch/arm/lib/crt0.S:80
80 bl board_init_f_alloc_reserve
(gdb)
board_init_f_alloc_reserve (top=9568000) at common/init/board_init.c:53
53 top = rounddown(top-sizeof(struct global_data), 16);
(gdb)
56 }
(gdb)
_main () at arch/arm/lib/crt0.S:81
81 mov sp, r0
(gdb)
_main () at arch/arm/lib/crt0.S:83
83 mov r9, r0
(gdb)
84 bl board_init_f_init_reserve
(gdb)
board_init_f_init_reserve (base=9566720) at common/init/board_init.c:111
111 memset(gd_ptr, '\0', sizeof(*gd));
(gdb)
101 {
(gdb)
111 memset(gd_ptr, '\0', sizeof(*gd));
(gdb)
memset () at arch/arm/lib/memset.S:24
24 ands r3, r0, #3 @ 1 unaligned?
(gdb)
25 mov ip, r0 @ preserve r0 as return value
(gdb)
26 bne 6f @ 1
(gdb)
30 1: orr r1, r1, r1, lsl #8
(gdb)
31 orr r1, r1, r1, lsl #16
(gdb)
32 mov r3, r1
(gdb)
33 cmp r2, #16
(gdb)
34 blt 4f
(gdb)
69 stmfd sp!, {r4-r8, lr}
(gdb)
memset () at arch/arm/lib/memset.S:70
70 mov r4, r1
(gdb)
71 mov r5, r1
(gdb)
72 mov r6, r1
(gdb)
73 mov r7, r1
(gdb)
74 mov r8, r1
(gdb)
75 mov lr, r1
(gdb)
77 cmp r2, #96
(gdb)
78 tstgt ip, #31
(gdb)
79 ble 3f
(gdb)
91 3: subs r2, r2, #64
(gdb)
92 stmiage ip!, {r1, r3-r8, lr}
(gdb)
93 stmiage ip!, {r1, r3-r8, lr}
(gdb)
94 bgt 3b
(gdb)
91 3: subs r2, r2, #64
(gdb)
92 stmiage ip!, {r1, r3-r8, lr}
(gdb)
93 stmiage ip!, {r1, r3-r8, lr}
(gdb)
94 bgt 3b
(gdb)
91 3: subs r2, r2, #64
(gdb)
92 stmiage ip!, {r1, r3-r8, lr}
(gdb)
93 stmiage ip!, {r1, r3-r8, lr}
(gdb)
94 bgt 3b
(gdb)
91 3: subs r2, r2, #64
(gdb)
92 stmiage ip!, {r1, r3-r8, lr}
(gdb)
93 stmiage ip!, {r1, r3-r8, lr}
(gdb)
94 bgt 3b
(gdb)
95 ldmfdeq sp!, {r4-r8, pc}
(gdb)
97 tst r2, #32
(gdb)
98 stmiane ip!, {r1, r3-r8, lr}
(gdb)
99 tst r2, #16
(gdb)
100 stmiane ip!, {r4-r7}
(gdb)
101 ldmfd sp!, {r4-r8, lr}
(gdb)
memset () at arch/arm/lib/memset.S:105
105 4: tst r2, #8
(gdb)
106 stmiane ip!, {r1, r3}
(gdb)
107 tst r2, #4
(gdb)
108 strne r1, [ip], #4
(gdb)
113 5: tst r2, #2
(gdb)
114 strbne r1, [ip], #1
(gdb)
115 strbne r1, [ip], #1
(gdb)
116 tst r2, #1
(gdb)
117 strbne r1, [ip], #1
(gdb)
118 ret lr
(gdb)
board_init_f_init_reserve (base=9566720) at common/init/board_init.c:117
117 base += roundup(sizeof(struct global_data), 16);
(gdb)
126 gd->malloc_base = base;
(gdb)
130 }
(gdb)
_main () at arch/arm/lib/crt0.S:86
86 mov r0, #0
(gdb)
87 bl board_init_f
(gdb)
board_init_f (boot_flags=0) at common/board_f.c:930
930 gd->have_console = 0;
(gdb)
929 gd->flags = boot_flags;
(gdb)
932 if (initcall_run_list(init_sequence_f))
(gdb)
930 gd->have_console = 0;
(gdb)
932 if (initcall_run_list(init_sequence_f))
(gdb)
initcall_run_list (init_sequence=init_sequence@entry=0x87870048 <init_sequence_f>) at lib/initcall.c:17
17 for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
(gdb)
14 {
(gdb)
17 for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
(gdb)
21 if (gd->flags & GD_FLG_RELOC)
(gdb)
22 reloc_ofs = gd->reloc_off;
(gdb)
27 if (gd->flags & GD_FLG_RELOC)
(gdb)
31 ret = (*init_fnc_ptr)();
(gdb)
^C
Program received signal SIGTRAP, Trace/breakpoint trap.
0xdeadbeee in ?? ()
(gdb) s
Cannot find bounds of current function
(gdb) s
Cannot find bounds of current function
(gdb)
So yeah, technically, I am able to debug U-boot but unable to pass first initialization procedures until any log message. But I am pretty sure that U-boot is correct as I am using it for a while!
Any ideas what is wrong?
Then I did following:
(gdb) load
Loading section .text, size 0x67458 lma 0x87800000
Loading section .rodata, size 0x14246 lma 0x87867458
Loading section .hash, size 0x18 lma 0x8787b6a0
Loading section .data, size 0x6ca4 lma 0x8787b6b8
Loading section .got.plt, size 0xc lma 0x8788235c
Loading section .u_boot_list, size 0x1208 lma 0x87882368
Loading section .efi_runtime, size 0x100 lma 0x87883570
Loading section .efi_runtime_rel, size 0x90 lma 0x87883670
Loading section .rel.dyn, size 0xd220 lma 0x87883700
Loading section .dynsym, size 0x30 lma 0x87890920
Loading section .dynstr, size 0x1 lma 0x87890950
Loading section .dynamic, size 0x90 lma 0x87890954
Loading section .gnu.hash, size 0x18 lma 0x878909e4
Start address 0x87800000, load size 592375
Transfer rate: 69 KB/sec, 12341 bytes/write.
(gdb) s
reset () at arch/arm/cpu/armv7/start.S:40
40 b save_boot_params
(gdb) delete
(gdb) b initcall_run_list
Breakpoint 1 at 0x87856dec: file lib/initcall.c, line 17.
(gdb) s
save_boot_params () at arch/arm/cpu/armv7/start.S:116
116 b save_boot_params_ret @ back to my caller
(gdb) c
Continuing.
Breakpoint 1, initcall_run_list (init_sequence=init_sequence@entry=0x87870048 <init_sequence_f>) at lib/initcall.c:17
17 for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
and yeah, I definitely debugging something but it fails on the early steps. Still can't understand what is wrong.
Hi Almaz
suggest to post on segger forum.
Best regards
igor