Hi,
I have SCU (CM4) debug port output from the UART and 2xCM4 UART serial access as well for the i.MX8QM EVK. Is there any serial output accessible from the AP cores (4xA53 and 2xA72) ? In other words, I don't see UART access for the AP cores. Is there some way for checking the start of any of the AP cores (A53 or A72) from the debug port or the SCU FW ?
Thanks in advance.
Hi ravi.kohli
it is possible to create image with enabled Cortex-A and Cortex-M4 in
various combinations as described on
i.MX8 Boot process and creating a bootable image
For uart one can check:
imx8qm_mek.h\configs\include - uboot-imx - i.MX U-Boot
imx8qm_mek.c\imx8qm_mek\freescale\board - uboot-imx - i.MX U-Boot
cpu.c\imx8\mach-imx\arm\arch - uboot-imx - i.MX U-Boot
example of starting m4 from linux
m4ctrl - M4 Control Tool for i.MX platforms
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------