I have spent some days to make a Debian8 system on SabreSD board, begins with Debian on the i.MX6 sabre sd platform in a few commands .
My code base is standard Yocto1.7 package "fsl-yocto-3.14.28-1.0.0" where 3D HW acceleration works fine when I run "es2_info" or demos in fsl_gpu_sdk.
For Linux kernel part, I keep debian same as yocto1.7.
For Rootfs, I move GFX relative libaries from "fsl-yocto-3.14.28-1.0.0", i.e. imx-gpu-viv, libdrm, mesa-demos, fsl-gpu-sdk, recompiling "xf86-video-imxfb-vivante" natively, set /etc/X11/xorg.conf as,
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "vivante"
Option "fbdev" "/dev/fb0"
Option "vivante_fbdev" "/dev/fb0"
Option "HWcursor" "false"
EndSection
then, Vivante xorg driver can make my LXDE desktop work happily. but when I run "es2_info", it prints
libEGLwarning: DRI2: falied to authenticate
EGL_VERSION: 1.4(DRI2)
EGL_VENDOR: Mesa Project
..........
GL_VERSION: OpenGL ES2.0 Mesa 10.6.3
GL_RENDERER: Software Rasterizer
.........
obviously, OpenGL ES is SW path. Please give some hints on how to enable HW path as Yocto1.7 does. Thanks.
Yours,
James
解決済! 解決策の投稿を見る。
Dear James,
I think vivante_drv.so comes from xserver-xorg-video-imx-viv package:
http://downloads.yoctoproject.org/mirror/sources/xserver-xorg-video-imx-viv-5.0.11.p4.4.tar.gz
Build:
BUILD_HARD_VFP=1 XSERVER_GREATER_THAN_13=1 BUSID_HAS_NUMBER=1 ./fastbuild.sh
./fastbuild.sh install
Regards,
Laszlo
Hello,
I have a working 3d acceleration in Debian 8. Here is a good starting point: http://pushpopmov.blogspot.hu/2015/01/vivante-gpu-drivers-on-imx6.html
The process I have made:
The last one is really a nasty workaround, but it works. I should have rebuilt Debian's Xorg from source but it failed. So if you are able to recompile a working Xorg binary please share the process.
Regards
Hi Laszlo Timko, is libglapi.so necessary for DRI HW acceleration? where do you get this file to your Debian system?
when my system has libglapi.so(.0.0.0) under usr/lib/arm-linu-gnueabihf/, the es2_info will report "Segmentation fault", if I remove it, es2_info shows "Xlib: extension "XFree86-DRI" missing on display ":0"", the remaining part of es2_info seems that HW acceleration is enabled, same as Yocto1.7's es2_info result. But when I run 3D demos such as es2gears_x11, the demo can run but nothing is shown in the window.
Thanks for your help in advance.
Dear James,
It seems to me that libglapi.so is not necessary for hw acceleration. I think I have the same file as you, but it is not relevant because this library is not loaded. I checked it with strace.
How does your Xorg.log file look like?
Hi Laszlo Timko, thanks for your great help. my Xorg.conf is as following, I am still struggling to make DRI work.
Section "ServerLayout"
Identifier "Default Layout"
Screen "Default Screen"
EndSection
Section "Module"
Load "dbe"
Load "extmod"
Load "freetype"
Load "glx"
Load "dri"
EndSection
Section "InputDevice"
Identifier "Generic Keyboard"
Driver "kbd"
Option "XkbLayout" "us"
Option "XkbModel" "pc105"
Option "XkbRules" "xorg"
EndSection
Section "InputDevice"
Identifier "Configured Mouse"
Driver "mouse"
Option "CorePointer"
EndSection
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "vivante"
Option "fbdev" "/dev/fb0"
Option "vivante_fbdev" "/dev/fb0"
Option "HWcursor" "false"
EndSection
Section "Monitor"
Identifier "Configured Monitor"
EndSection
Section "Screen"
Identifier "Default Screen"
Monitor "Configured Monitor"
Device "i.MX Accelerated Framebuffer Device"
DefaultDepth 24
EndSection
Section "DRI"
Mode 0666
EndSection
And the result of es2_info is,
Xlib: extension "XFree86-DRI" missing on display ":0".
Xlib: extension "XFree86-DRI" missing on display ":0".
Xlib: extension "XFree86-DRI" missing on display ":0".
EGL_VERSION: 1.4
EGL_VENDOR: Vivante Corporation
EGL_EXTENSIONS:
EGL_KHR_reusable_sync, EGL_KHR_fence_sync, EGL_KHR_image,
EGL_KHR_image_base, EGL_KHR_image_pixmap, EGL_KHR_gl_texture_2D_image,
EGL_KHR_gl_texture_cubemap_image, EGL_KHR_gl_renderbuffer_image,
EGL_KHR_lock_surface, EGL_KHR_create_context,
EGL_EXT_create_context_robustness, EGL_EXT_buffer_age,
EGL_EXT_protected_surface
EGL_CLIENT_APIS: OpenGL_ES OpenVG
GL_VERSION: OpenGL ES 3.0 V5.0.11.p4.25762
GL_RENDERER: Vivante GC2000
GL_EXTENSIONS:
GL_OES_vertex_type_10_10_10_2, GL_OES_vertex_half_float,
GL_OES_element_index_uint, GL_OES_mapbuffer, GL_OES_vertex_array_object,
GL_OES_compressed_ETC1_RGB8_texture, GL_OES_compressed_paletted_texture,
GL_OES_texture_npot, GL_OES_rgb8_rgba8, GL_OES_depth_texture,
GL_OES_depth_texture_cube_map, GL_OES_depth24, GL_OES_depth32,
GL_OES_packed_depth_stencil, GL_OES_fbo_render_mipmap,
GL_OES_get_program_binary, GL_OES_fragment_precision_high,
GL_OES_standard_derivatives, GL_OES_EGL_image, GL_OES_EGL_sync,
GL_EXT_texture_type_2_10_10_10_REV, GL_EXT_texture_filter_anisotropic,
GL_EXT_texture_format_BGRA8888, GL_EXT_read_format_bgra,
GL_EXT_multi_draw_arrays, GL_EXT_frag_depth, GL_EXT_discard_framebuffer,
GL_EXT_blend_minmax, GL_EXT_multisampled_render_to_texture,
GL_EXT_robustness, GL_VIV_tex_direct
Dear James,
Please share your Xorg.log instead of conf.
Es2_info output seems ok, but of course I don't get those XFree86-DRI error lines.
Have you removed libEGL, libGLESv2, libGL libraries from /usr/lib/arm-linux-gnueabihf?
Cheers
Dear Laszlo, Thanks a lot for your help, With your files, the 3D WORKS!!!
My vivante_drv.so will cause "segment fault" issue, but yours will not. May I know how you compile the xorg driver? my steps are as following,
apt-get install build-essential
apt-get install xserver-xorg-dev libxext-dev
tar -zxvf imx-gpu-viv_1_5.0.11.p4.4-hfp.tar.gz -C /
following build document in the tar package, please don't set YOCTO=1.
The EXA works fine but DRI fails.
Thanks again.
BRs,
James
Dear James,
I think vivante_drv.so comes from xserver-xorg-video-imx-viv package:
http://downloads.yoctoproject.org/mirror/sources/xserver-xorg-video-imx-viv-5.0.11.p4.4.tar.gz
Build:
BUILD_HARD_VFP=1 XSERVER_GREATER_THAN_13=1 BUSID_HAS_NUMBER=1 ./fastbuild.sh
./fastbuild.sh install
Regards,
Laszlo
Dear Laszlo, YES! With your great help, I finally found that I didn't add BUILD_HARD_VFP=1, because the document said" for kernel 3.5.7, use "BUSID_HAS_NUMBER=1"" but I am using 3.14 kernel. besides my careless, I do think freescale guys should update their document for avoiding any missunderstanding.
Thanks again for your help!
BRs,
James
Dear Laszlo,
Sorry to bother you again, I just returned to this project recentlly, but I find while 3D apps running on debian8, mouse clicking on somewhere else will cause system hang randomly, have you ever met this issue?
BRs,
James
Hi,
Strange. I have never experienced this kind of issue.
Laszlo
Hi Laszlo Timko, lots of thanks to your sharing, I will try your solution soon.
The way to native build Xorg driver is:
apt-get install build-essential
apt-get install xserver-xorg-dev libxext-dev
tar -zxvf imx-gpu-viv_1_5.0.11.p4.4-hfp.tar.gz -C /
following build document in the tar package, please don't set YOCTO=1.
I didn't build xorg server from source code either.
I just tried to copy libEGL.so* /libGLES*.* from /usr/lib/ to /usr/lib/arm-linux-gnueabihf/,
the es2_info reports "Segmentation fault", maybe this operation has some relative to my issue. I will continue to dig.