De-interlace Capture using V4L in Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

De-interlace Capture using V4L in Yocto

1,052 Views
ko-hey
Senior Contributor II

Hi all

I'm trying to do de-interlace V4L2 capture with patch that was provided in following community.

De-interlace Capture Device​​

But it's not work well.

For example, it's shown a blur on the image after de-interlace.

I think the patch is for Ltib, so it's not appropriate for Yocto Linux.

Does anyone have a patch for Yocto Linux ?

If yes, please share it.

Also if anyone have experience that operate de-interlace V4L2 capture in Yocto, please let me know how to do.

Ko-hey

Labels (2)
0 Kudos
Reply
1 Reply

467 Views
b36401
NXP Employee
NXP Employee

We have no any de-interlace patch other than that one.

Sorry for the inconvenience.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply