Hello, I have a question about databases. I need to install PostgreSQL on i.MX28, in which application will write data. I download postgresql-9.3.5.tar.bz2 from postgresql.org, install it in rootfs directory of LTIB. Then I create new database, and write into it three rows. Then I wrote SD card and launch i.mx. But when I try to launch any of scripts of pgsql, I get only errors.
root@freescale /pgsql/bin$ ./psql
./psql: line 1: syntax error: unexpected "("
root@freescale /pgsql/bin$ ./postgres
./postgres: line 1: syntax error: unexpected "("
And application can't connect to db too.
I tried to connect to db from application on windows, everything ok.
So, how can I start the PostgreSQL server on i.mx? Or there is something wrong?
And I also create a new user Admin to launch postgresql (because it is impossible to launch it under root), so should I create another user on i.mx?
Maybe there is another way of installation PostgreSQL on i.mx? With LTIB and .spec?
Thanks in advance.
Okay, thank you for your answers. But I need to install PostgreSQL. Well, I should compile it from sources. That sounds good, but I don't know how) Please, could you give me any advices how to do it? Becaue I have no idea
To do that, first you need to download PostgreSQL source files.
For example you can get them from their official site:
And then you need to compile them on your host PC using cross compiler.
You can use toolchain from LTIB.
Or may try using use CodeSourcery (Mentor) toolchain on Windows host:
http://www.mentor.com/embedded-software/codesourcery
http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/editions/lite-edition/
Alternativelly you can compile PostgreSQL directly on the board if you install gcc there.
However I suppose this way is worse.
I just tried to compile with LTIB. I downloaded postgresql-9.3.5.tar.bz2 from their site and put it into rpm/SOURCES, and created in dist/lfs-5.1 directory postgresql with file postgresql.spec in it. File contains:
%define pfx /opt/freescale/rootfs/%{_target_cpu}
Summary : PostgreSQL for arm
Name : postgresql
Version : 9.3.5
Release : 1
License :
Vendor : PostgreSQL
Packager :
Group : System Environment/Libraries
URL : http://
Source : %{name}-%{version}.tar.bz2
BuildRoot : %{_tmppath}/%{name}
Prefix : %{pfx}
%Description
%{summary}
%Prep
%setup
%Build
./configure --prefix=%{_prefix} --host=$CFGHOST --build=%{_build}
make
%Install
rm -rf $RPM_BUILD_ROOT
make install DESTDIR=$RPM_BUILD_ROOT/%{pfx}
%Clean
rm -rf $RPM_BUILD_ROOT
%Files
%defattr(-,root,root)
%{pfx}/*
After ./ltib -p postgresql.spec I get errors:
checking for zic... no
configure: error:
When cross-compiling, either use the option --with-system-tzdata to use
existing time-zone data, or set the environment variable ZIC to a zic
program to use during the build.
error: Bad exit status from /home/ubuntu/Projects/TionPro28/ltib/ltib/tmp/rpm-tmp.2856 (%build)
I think, my .spec file is bad, could you help me to create correct .spec? Or may be give an advise about it?
I think, Buildroot (http://buildroot.org/download.html) contains that PostgreSQL, which is needed for i.mx28. But is it possible to take it from there and past into rootfs of ltib?
I suspect that you actually installed x86 PostgreSQL on your PC.
Such outputs
> ./psql: line 1: syntax error: unexpected "("
> ./postgres: line 1: syntax error: unexpected "("
mean that Linux OS running on the board does not recognize
psql and postgres as executable binaries and tryes to run them
as scriprs. It suggests me that psql and postgres are actually
x86 binaries.
Please check it with "file" utility such way. Here busybox
is i.MX28 binary and /bin/bash is x86 one:
vik@tecno:~/ltib/1012-28/ltib-perl/rootfs/bin$ file busybox
busybox: setuid ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), stripped
vik@tecno:~/ltib/1012-28/ltib-perl/rootfs/bin$ file /bin/bash
/bin/bash: ELF 32-bit LSB executable, Intel 80386, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.15, stripped
vik@tecno:~/ltib/1012-28/ltib-perl/rootfs/bin$
If so you need to get PostgreSQL compiled for right architecture
or compile it from sources yourself.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------