Hi,
I am facing strange issue where in I see that the framebuffer fb does not gets registered when I give disp_dev as "mipi_dsi". On other hand, when I use this disp_dev as "lcd" fb registers. This piece of code was working earlier for me, and now I am not getting why even the fb is not registered.
Changes I have done in File imx6qdl_sabreauto.dtsi:
mxcfb3: fb@2 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "mipi_dsi";
interface_pix_fmt = "RGB666";
mode_str ="TRULY-WVGA";
default_bpp = <24>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
mipi_dsi_reset: mipi-dsi-reset {
compatible = "gpio-reset";
reset-gpios = <&gpio6 11 GPIO_ACTIVE_LOW>;
reset-delay-us = <50>;
#reset-cells = <0>;
};
reg_mipi_dsi_pwr_on: mipi_dsi_pwr_on {
compatible = "regulator-fixed";
regulator-name = "mipi_dsi_pwr_on";
gpio = <&gpio6 14 0>;
enable-active-high;
};
&mipi_dsi {
compatible = "fsl,imx6dl-mipi-dsi";
reg = <0x021e0000 0x4000>;
interrupts = <0 102 0x04>;
gpr = <&gpr>;
clocks = <&clks 138>, <&clks 204>;
clock-names = "mipi_pllref_clk", "mipi_cfg_clk";
dev_id = <0>;
disp_id = <0>;
lcd_panel = "TRULY-WVGA";
disp-power-on-supply = <®_mipi_dsi_pwr_on>;
resets = <&mipi_dsi_reset>;
status = "okay";
};
All other Fbs are disabled. Any hints will be very helpful.
Thanks and regards
Kunal
解決済! 解決策の投稿を見る。
Hi Igor,
Thanks for response. Yes, I was missing few things there. The clock frequency configured in the driver was not the one matching with the table. So due to uninitialization of the disp_dev the fb was not getting enabled.
Thanks and regards,
Kunal
Hi Kunal
one can check if mipi-dsi driver is included in build configuration,
please refer to sect.7.3.2 Menu Configuration Options
attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for response. Yes, I was missing few things there. The clock frequency configured in the driver was not the one matching with the table. So due to uninitialization of the disp_dev the fb was not getting enabled.
Thanks and regards,
Kunal