Hi,
We are new to iMx8dx/qxp processors, We are looking GPIO configuration for DTS file for the different peripherals
Could you please help me any tool or application to configure the GPIO's for iMX8dx and iMX8qxp processors.
Regards,
Viswa
Hi,
1.
We installed PIN tool but IMX8dx/qxp database didn't find.
https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX
2. fsl-imx8dx.dtsi : has imx8qm only.
gpio1: gpio@5d090000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d090000 0x0 0x10000>;
interrupts = <GIC_SPI 137 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio1>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio2: gpio@5d0a0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0a0000 0x0 0x10000>;
interrupts = <GIC_SPI 138 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio3: gpio@5d0b0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0b0000 0x0 0x10000>;
interrupts = <GIC_SPI 139 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio3>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio4: gpio@5d0c0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0c0000 0x0 0x10000>;
interrupts = <GIC_SPI 140 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio4>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio5: gpio@5d0d0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0d0000 0x0 0x10000>;
interrupts = <GIC_SPI 141 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio5>;
interrupt-controller;
#interrupt-cells = <2>;
};
3#: NO DRIVER FOR GPIOS
didnt find the gpio driver in the kernel in "/drivers/gpio/"
which has got errors: Not able to export. any GPIO.
[ 115.430117] export_store: invalid GPIO 73 [ 184.114083] export_store: invalid GPIO 105 [ 342.974089] export_store: invalid GPIO 73
4#: GPIO DTS file config.
Please correct me if my DTS file config is wrong:
GPIO3_IO13 Output
GPIO3_IO09 Output
GPIO3_IO10 Output
GPIO3_IO11 Input / Open drain ?
GPIO3_IO12 Input / Open drain ?
GPIO3_IO18 Output
GPIO1_IO20 Output
GPIO1_IO19 Output
GPIO1.IO13 Input - ADC Input <--ADC
few GPIOs are INPUT and few are OUTPUT.
fsl,pins = <
SC_P_QSPI0A_DQS_LSIO_GPIO3_IO13 0x20000021 as a Output is thos config value is correct ??
SC_P_QSPI0A_DATA0_LSIO_GPIO3_IO09 0x20000021
SC_P_QSPI0A_DATA2_LSIO_GPIO3_IO11 0x24000021 /* No pullup, OPEN_DRAIN_INPUT, LSIO_GPIO3_IO11*/
SC_P_QSPI0A_DATA3_LSIO_GPIO3_IO12 0x24000021 /* No pullup, OPEN_DRAIN_INPUT, LSIO_GPIO3_IO11*/
SC_P_QSPI0B_DATA0_LSIO_GPIO3_IO18 0x20000021
/*SC_P_FLEXCAN2_TX_LSIO_GPIO1_IO20 0x00000021 */
SC_P_FLEXCAN2_RX_LSIO_GPIO1_IO19 0x20000021
SC_P_ADC_IN5_ADMA_ADC_IN5 0x04000006 /*Drive select 12mA, OPEN_DRAIN_INPUT, ADMA_ADC_IN5 */
>;
Regards,
Viswa
I don't understand these addresses ... Cannot match IMX8 user guide and GPIO blocks addresses to what this Linux DTS has..
How does this work .? What is at 5d09000, GPIO1 starts at 0x30200000 etc ..
gpio1: gpio@5d090000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d090000 0x0 0x10000>;
interrupts = <GIC_SPI 137 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio1>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio2: gpio@5d0a0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0a0000 0x0 0x10000>;
interrupts = <GIC_SPI 138 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio3: gpio@5d0b0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0b0000 0x0 0x10000>;
interrupts = <GIC_SPI 139 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio3>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio4: gpio@5d0c0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0c0000 0x0 0x10000>;
interrupts = <GIC_SPI 140 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio4>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio5: gpio@5d0d0000 {
compatible = "fsl,imx8qm-gpio", "fsl,imx35-gpio";
reg = <0x0 0x5d0d0000 0x0 0x10000>;
interrupts = <GIC_SPI 141 IRQ_TYPE_LEVEL_HIGH>;
gpio-controller;
#gpio-cells = <2>;
power-domains = <&pd_lsio_gpio5>;
interrupt-controller;
#interrupt-cells = <2>;
};
adf
Hello Viswa,
Are you using the latest version of the Pins Tool? Please also make sure that the tool can connect to the internet. Sometimes you may not see the processor’s information if the tool cannot connect to the repositories to fetch the processor configuration.
I checked, and the configurations are available on the repository with the correct device tree code so you should be able to access it.
Regards,
Hello Viswa,
You may use the latest version of the Pins Tool for i.MX. The processor information is fetched by the application so please make sure that the tool has internet access.
https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX
This tool has a GUI and allows you to configure the muxing options and to generate the Device Tree code for your hardware.
I hope this helps,
Regards,