DO254 compliance support for IMX6/IMX8 processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DO254 compliance support for IMX6/IMX8 processors

878件の閲覧回数
sarath831989
Contributor I

Hi i am planning to use IMX6/IMX8 series processor in aero design. I need to know whether the processor is complied to DO254 or is there any reference where the processor being used in aero based design earlier. 

Also, is it possible for NXP to provide support to comply the processor with DO-254 standard. 

タグ(1)
0 件の賞賛
1 返信

639件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Sarath Babu Govinda Babu,

Some i.MX Processors part numbers comply with Automotive or Industrial standards, which may overlap with the requirements for airborne electronic hardware.

There is a document that lists some of the recommendations for these applications:

Freescale Recommendations for Avionic and Defense Applications

https://community.nxp.com/docs/DOC-104735

If you have any doubts about a specific requirement I would recommend contacting your FAE or Distributor for more detailed information.

I hope this helps!

Regards,

0 件の賞賛