DDR3 data lines swapped , imx6 solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 data lines swapped , imx6 solo

237 Views
SUV
Contributor I

We are working on imx6 solo board. Due to hardware space constraint, the data lines between DDR3 controller (IS43TR16256B-125KBL) and imx6 solo processor (MCIMX6S5EVM10AD) are swapped.

Data bit D11 from DDR3 controller is connected to Data bit D14 of imx6 solo processor and Data bit D14 from DDR3 controller is connected to Data bit D11 of imx6 solo processor.

For the lines swapped, what changes are we supposed to do for DDR3 control registers ?
or any changes in Board support package?


0 Kudos
1 Reply

205 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @SUV,

I hope you are doing well.

There is no requirement for any specific control register changes.

For more information, please refer to the link given below:
https://community.nxp.com/t5/i-MX-Processors/ddr3-data-lines-swapped-imx6sl/m-p/324402

Thanks & Regards,
Ritesh M Patel

0 Kudos