Hi,
we have the same DDR3 config like the SABRESDB. Also the Layout is the same. Also the memory is mircron, but the low voltage version. We are using the Stress Test tool from Freescale but a lots of our boards don't pass the calibration. What can I do? What I have to config to solve this or where can I find the cause of this issue. Are there better tools like the Stress Test tool?
Regards Marcel
解決済! 解決策の投稿を見る。
So I have found the issue, the write leveling setting are false.
setmem /32 0x021b080c = 0x001F001F
setmem /32 0x021b0810 = 0x001F001F
setmem /32 0x021b480c = 0x00440044
setmem /32 0x021b4810 = 0x00440044
But you have to set for T-Routing all four equal
setmem /32 0x021b080c = 0x001F001F
setmem /32 0x021b0810 = 0x001F001F
setmem /32 0x021b480c = 0x001F001F
setmem /32 0x021b4810 = 0x001F001F
Hi, Marcel
You can refer to https://community.freescale.com/docs/DOC-94917 to update your DDR scripts.
Regards,
Tao Zheng
Hi,
Thank you, that s a good idea. But for some i.MX6 we dont get some calibrartion results to fill in, because I get a ERROR message at DQS gating calibration.
Regards
Marcel
What do you mean? Can't you use Mx6DQSDL DDR3 Script Aid V0.08 to generate your DDR scripts?
So I have found the issue, the write leveling setting are false.
setmem /32 0x021b080c = 0x001F001F
setmem /32 0x021b0810 = 0x001F001F
setmem /32 0x021b480c = 0x00440044
setmem /32 0x021b4810 = 0x00440044
But you have to set for T-Routing all four equal
setmem /32 0x021b080c = 0x001F001F
setmem /32 0x021b0810 = 0x001F001F
setmem /32 0x021b480c = 0x001F001F
setmem /32 0x021b4810 = 0x001F001F
Hi I mean, I can t fill in the calibration data I get nothing back from the tool with the sabre data because
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
The DDR stress test can run with an incrementing frequency or at a static freq
To run at a static freq, simply set the start freq and end freq to the same valu