DDR3 Signal length in i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR3 Signal length in i.MX6Q

跳至解决方案
1,619 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to Table 3-5. Total signal etch (DDR3) in Hardware Development Guide for i.MX6DQ6SDL, Rev. 1.

There is description of DRAM_SDCLK0 : 2120.044[Mils].

My customer measured the DRAM_SDCLK0 length on i.MX6Q SABRE-AI.

Actually the DRAM_SDCLK0 length looked 1849.483[Mils].

Refer to attached file: "DDR3_SDCLK_Length.xlsx"

[Question]

Should we think including the branch wiring about each signal length?

Or, can we ignore the branch wiring length?

BR,

Keita

标签 (5)
0 项奖励
回复
1 解答
1,417 次查看
art
NXP Employee
NXP Employee

Hi Keita,

No, you have not to include the length of the wire branches you've shown into the total trace length calculation from the processor to the DDR3 chip.

Best Regards,

Artur

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,417 次查看
art
NXP Employee
NXP Employee

Yes, the trace length within a via should be taken into the account when calculating total trace length. However, only the actual trace length should be taken into the account, not always a total board thickness. For example, if a trace goes from Layer 2 to Layer 6 through a via on 8-layer board, only the distance between Layer 2 and Layer 6 should be taken into the account, not total board thickness.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,417 次查看
keitanagashima
Senior Contributor I

Hi Artur,

Thank you for your reply.

I'd like to know about branched wire when calculating total trace length.

Refer to attached file.

Should we consider the branched wire to calculate total trace length?

Best Regards,

Keita

0 项奖励
回复
1,418 次查看
art
NXP Employee
NXP Employee

Hi Keita,

No, you have not to include the length of the wire branches you've shown into the total trace length calculation from the processor to the DDR3 chip.

Best Regards,

Artur

0 项奖励
回复
1,417 次查看
keitanagashima
Senior Contributor I

Hi Artur,

Thank you for your reply.

OK. I got it!

BR,

Keita

0 项奖励
回复