Total memory is 4G bytes, 8G bits Dual Die (2CS) * 4.
Detail log as attachments.
------------------------------------------------------------------
Would you like to run the write leveling calibration? (y/n)
Please enter the MR1 value on the initilization script
This will be re-programmed into MR1 after write leveling calibration
Enter as a 4-digit HEX value, example 0004, then hit enter
0000 You have entered: 0x0000
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x000D000B
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x0012000D
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00040012
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x017E000F
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
------------------------------------------------------------------
Would you like to run the write leveling calibration? (y/n)
Please enter the MR1 value on the initilization script
This will be re-programmed into MR1 after write leveling calibration
Enter as a 4-digit HEX value, example 0004, then hit enter
0004 You have entered: 0x0004
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x000E0006
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00150010
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00040016
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x017F000F
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
------------------------------------------------------------------
Original Attachment has been moved to: imx6q_4g.inc.zip
Original Attachment has been moved to: mx6q_4g_ddr_stress_test_3.log.zip
Original Attachment has been moved to: mx6q_4g_ddr_stress_test.log.zip
Please try using DDR_Stress_Tester_V1.0.3
https://community.freescale.com/docs/DOC-96412
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------