The DDR on imx6ull evalution board showing part number as D9SHD. How to figure it out what is the physical size of DDR. Could please help me in figuring out the size of DDR.
Thanks, Jaya
Hi Jaya
one can look at i.MX6ULL EVK design files (schematic, BOM)
Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
MCIMX6ULL-EVK_DESIGNFILES
http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/ev...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have checked with the above part number in micron website (FBGA & Component Marking Decoder )it is showing as 256mb.
But in U-boot it is showing as below.
---------
U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Apr 24 2018 - 13:31:40 +0530)
CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 37C
Reset cause: POR
Model: Freescale i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
-------------
What are the code changes I need to do, so that it can display as the actual size i.e. 256MB in Uboot, for MT41K256M16TW(256MB) DDR chip.
Could please help me in this regard. Waiting for your reply.
Thanks ,
Jaya
could you try with Demo Images
Best regards
igor
Hi Igor,
I have tried with given above images, still u-boot shows 512MB.
See the below logs:
----------------------
--------------------------
What are the code changes I need to do, so that it can display as the actual size i.e. 256MB in Uboot, for MT41K256M16TW(256MB) DDR chip.
Could you please help me.
Thanks,
Jaya
Hi Igor,
I have already changed the value for PHYS_SDRAM_SIZE as 256 MB, but it is not updating from here for uboot.
See the below code from which the size of DDR is getting updated in u-boot. Could you please share me how to get
ctl and misc values for MT41K256M16TW(256MB) DDR chip.
unsigned imx_ddr_size(void)
{
struct esd_mmdc_regs *mem = (struct esd_mmdc_regs *)MEMCTL_BASE;
unsigned ctl = readl(&mem->ctl);
unsigned misc = readl(&mem->misc);
int bits = 11 + 0 + 0 + 1; /* row + col + bank + width */
bits += ESD_MMDC_CTL_GET_ROW(ctl);
bits += col_lookup[ESD_MMDC_CTL_GET_COLUMN(ctl)];
bits += bank_lookup[ESD_MMDC_MISC_GET_BANK(misc)];
bits += ESD_MMDC_CTL_GET_WIDTH(ctl);
bits += ESD_MMDC_CTL_GET_CS1(ctl);
}
Could you please help me in this regard. This will be a great help as I am struck for long time in this.
Thanks ,
Jaya
Hi Jaya
you can try to recheck memory settings generating ddr script, then rebuild uboot
put new settings to uboot/board/../mx6ullevk/imximage.cfg
Best regards
igor