Dear Team,
I wanted to test DDR calibration on imx6. Testing only for Write leveling, DQS, Read/write leveling.
DDR start address s 0X10000000 DDR size 2GB.
in this DDR3 allocations :
cached ram size is : DDR base addr + 2GB - 1MB
uncached ram is : last 1MB
pagetable is placed at end of the cached ram.
when running the DDR calibration tests, I got the following error.
=============================STARTING DDR CALIBRATION=============================
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x002C001F
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x002C002A
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00240033
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0016002A
Starting DQS gating calibration...
**Memory did not transfer correctly, DDRtest_SSN_memcpy2 failed
...
We are using 64-bit DDR3 memory, here we observe that CSD0_base_address and some other variable content is lost/overwriting with some garbage value. while executing the tests.
Can you please suggest the problem solution.
解決済! 解決策の投稿を見る。
Hi ALL,
I have changed some of the drive strength parameters in DDR config code, all tests are passing.
But I configured Write levelling parameters as:
0x021b080c = 0x001F001F
0x021b0810 = 0x001F001F
0x021b480c = 0x001F001F
0x021b4810 = 0x001F001F
and output values are:
Start write leveling calibration
Write leveling calibration completed
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x004E0051
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00420048
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00330031
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0030003F
could please help me, the output values are larger than configured values?
Do i need to change any configuration parameters.
Please suggest me.
Hi ALL,
I have changed some of the drive strength parameters in DDR config code, all tests are passing.
But I configured Write levelling parameters as:
0x021b080c = 0x001F001F
0x021b0810 = 0x001F001F
0x021b480c = 0x001F001F
0x021b4810 = 0x001F001F
and output values are:
Start write leveling calibration
Write leveling calibration completed
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x004E0051
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00420048
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00330031
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0030003F
could please help me, the output values are larger than configured values?
Do i need to change any configuration parameters.
Please suggest me.
Hi DHANUNJAY
If the value of any of the WL_DL_ABS_OFFSETn [MPWLDECTRL0] register fields
are greater than ‘1F’, WALAT should be set to ‘1’ .
WALAT should be further increased for any full cycle delays added by the
WL_CYC_DELn register fields.
For "SSN_memcpy2" error recommended to test memory with lower ddr/cpu
frequencies, as this may be caused by board noise.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Greetings!
Thanks for very quick response!!
After changing WALT to 1 and write 0x021b0018 = 0x00011740
Then also same issue is repeating:
=============================STARTING DDR CALIBRATION=============================
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x002A001F
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x002C0028
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00250031
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x00140029
Starting DQS gating calibration...
**Memory did not transfer correctly, DDRtest_SSN_memcpy1 failed
**Memory did not transfer correctly, DDRtest_SSN_memcpy2 failed
. . .
Any other inputs?
We are running CPu at 600Mhz
and DDR3 @ 400Mhz.
Hi DHANUNJAY
one can tweak drive strength settings, this may be done
both on i.MX6 and DDR side.
~igor
Hi Igor,
Greetings!!
I tried with all combinations/drive parameters but no luck.
I observed, while executing ddr_calibration_sw( 0x00,0x02); It prforms internally memcpy() op, the (CSD0_BASE_ADDRESS=0x10000000) variable value becomes zero.how it is possible, the DDR testcode in IRAM.
How this value becomes zero?
If i declare macro, it will throwing errors like **Memory did not transfer correctly, DDRtest_SSN_memcpy2 failed.
Please give your suggestion on this.
Thanks,
Dhanunjay
Hi Dhanujay
test should show info like:
Address of test2 failure: Data was: | But pattern was: |
based on that one can check fault bits (pattern) with oscilloscope.
Further one can slow down ddr frequency.
If this will not help, attach jtag and write the same pattern with jtag,
again controlling waveforms with oscilloscope.
Best regards
igor
Hi,
Here is log:
Data was: 0xE59FF01CE59FF01C
But pattern was: 0xAAAAAAAAAAAAAAAA
Source is wrong, it is: 0x02C6D7E600000450
Address ÿË
á55)éÁáÁÁåÅÝÕÉ
write leveling is passed, but ddr_calibration_sw() failed.