Hello All,
I am developing V4L2 image sensor driver for a custom sensor.
Platform details are:
Board : HummingBoard-i2eX (i.MX6 Dual)
OS : Ubuntu, Linux Kernel 3.0.35
Sensor details:
1. Supported MIPI lanes : 2 Lane/4 Lane (configured to use 2 lane mode)
2. Supported MIPI data format : RAW 10 /RAW8 (configured to use RAW10)
3. Virtual channel : configured to 0
4. Clock Frequency : 24MHz (This is actually sensor clock, MIPI clock is 114 MHz)
5. Resolution : 1280 x 720
I am getting error "ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0" for VIDIOC_DQBUF IOCTL.
To begin my trouble shooting, I would like to get my below board configuration file modifications reviewed:
//Sensor details
static struct fsl_mxc_camera_platform_data mipi_csi2_data = {
.mclk = 24000000, // Is this OK ? Or should I put the MIPI clock(114 MHz) here?
.mclk_source = 0, // Does this indicate HB MIPI clock source is sensor?
.csi = 0, // Does this indicate camera sensor is using IPU #1/CSI0 ?
.io_init = mx6q_csi0_io_init, // I use this function to Enable mipi to IPU1 CSI0 (mxc_iomux_set_gpr_register(1, 19, 1, 0))
};
Since this structure definition doesn't have any documentation, I did not understand the meaning of these parameters. Please explain me these parameters if anybody is aware of.
//Details of MIPI CSI2 interface
static struct mipi_csi2_platform_data mipi_csi2_pdata = {
.ipu_id = 0,
.csi_id = 0,
.v_channel = 0,
.lanes =2,
.dphy_clk = "mipi_pllref_clk",
.pixel_clk = "emi_clk",
};
/*Details of capture device*/
static struct fsl_mxc_capture_platform_data capture_data[] = {
{
.csi = 0,
.ipu = 0,
.mclk_source = 0,
.is_mipi = 1,
},
};
Actually, I took these values from another sensor patch, i dont really know what these parameters are
Now, assuming that my board configuration is ok, I went ahead with driver debugging. Below are the observations:
1. I2C communication is ok
2. MIPI_CSI_PHY_STATE value is : 630,sometimes 330,300 also (Is this ok or is it indicating any clock related issue?)
3. MIPI_CSI_ERR1/2 both return 0
Any hints to my issue? Can this be related to the format my sensor support (RAW 10)? Can someone direct me how to proceed with debugging?
Also, in mxc_mipi driver, I saw apis to read MIPI_CSI_PHY_STATE and MIPI_CSI_ERR1/2 registers,however, I didnt find any apis to read other registers
(MIPI_CSI_N_LANES ~ MIPI_CSI_DATA_IDS_2). Can someone guide me on how to read the other registers (also, IPU registers) ?
解決済! 解決策の投稿を見る。
Update:
1. I got the issue resolved by switching to latest kernel (3.14 FSL) and adding some basic RAW10 support in BSP.
2. Also, I had to set p->if_type as V4L2_IF_TYPE_BT656 (V4L2_IF_TYPE_BT656_PROGRESSIVE did not work,don't know the reason ) in ioctl_g_ifparm of the sensor driver.
Update:
1. I got the issue resolved by switching to latest kernel (3.14 FSL) and adding some basic RAW10 support in BSP.
2. Also, I had to set p->if_type as V4L2_IF_TYPE_BT656 (V4L2_IF_TYPE_BT656_PROGRESSIVE did not work,don't know the reason ) in ioctl_g_ifparm of the sensor driver.
Hi Rejeesh Babu,
1. I got the issue resolved by switching to latest kernel (3.14 FSL) and adding some basic RAW10 support in BSP.
Raw10 data can be displayed on the imx6?(not use ISP/DSP)
Hi @ken meng,
I have managed to store frames from ov9724 camera to memory using the following command.
./mxc_v4l2_capture.out -iw 1280 -ih 720 -ow 1280 -oh 720 -m 1 -i 1 -r 0 -c 10 -fr 30 -d /dev/video1 /mnt/4.data
I am also attaching the camera data file here. How do I go about converting it to RGB? It is in the IPU Generic format.
Actually, the camera streams it in RAW-10 format, but I configured the IPU for V4L2_PIX_FMT_SBGGR10 format, which the IPU detects as IPU_PIX_FMT_GENERIC format. I am unsure as to how to go about processing the raw images. How to verify if the data saved in the file is in the correct format?
I am attaching the hex dump of the data from the frame file. Seems that every 3rd and fourth lines (one line = 16byte) are the same. Does this look like a valid raw data image?
00000000 89 24 07 1f c7 1f 88 21 c7 1e c8 22 48 20 c7 1f |.$.....!..."H ..|
00000010 c7 1e 4a 2b 48 22 09 26 48 20 49 26 c8 21 09 26 |..J+H".&H I&.!.&|
00000020 d4 50 0b 2f 15 54 cd 34 91 47 8b 2f 11 46 4c 33 |.P./.T.4.G./.FL3|
*
00000040 c7 1d 4a 29 48 22 49 27 48 22 08 20 88 23 88 21 |..J)H"I'H". .#.!|
00000050 08 21 89 26 c8 21 09 25 48 20 08 21 86 1b c8 23 |.!.&.!.%H .!...#|
00000060 13 4d 0e 38 11 46 4b 2d 51 47 4b 2c d0 41 4e 39 |.M.8.FK-QGK,.AN9|
*
00000080 48 22 09 27 87 1d c8 22 c7 1c 49 24 87 1d 08 21 |H".'..."..I$...!|
00000090 88 22 88 20 47 1f c8 21 c6 19 48 22 87 1e 87 1e |.". G..!..H"....|
000000a0 10 41 4a 2a 11 44 cb 2f 11 46 0c 30 0f 3d 8c 30 |.AJ*.D./.F.0.=.0|
*
000000c0 c6 1a 87 1e c7 1c 46 1a 87 1f 89 24 07 1e c8 20 |......F....$... |
000000d0 86 1b c7 1d c6 1a 08 23 47 1e 07 1d 47 1c 88 23 |.......#G...G..#|
000000e0 4f 3f 4c 32 14 50 8b 2f 91 47 8e 39 d1 46 cd 34 |O?L2.P./.G.9.F.4|
*
00000100 c9 25 09 25 08 22 4b 2c 08 21 0a 2a c9 27 8b 2e |.%.%."K,.!.*.'..|
00000110 49 26 cc 33 8a 2a 49 27 49 27 4a 29 c8 22 ca 29 |I&.3.*I'I'J).".)|
00000120 d1 46 cd 35 94 51 8e 39 54 52 8c 33 51 46 4d 37 |.F.5.Q.9TR.3QFM7|
*
00000140 07 1e 4a 2a 4a 29 89 25 09 26 8b 2d 49 25 ca 2a |..J*J).%.&.-I%.*|
00000150 4a 28 8a 29 0a 28 49 26 8a 28 8b 2c 0a 29 49 27 |J(.).(I&.(.,.)I'|
00000160 56 59 8e 38 94 51 0d 37 53 4f 8f 3c 14 51 4e 38 |VY.8.Q.7SO.<.QN8|
Hi All,
Assuming that my problem is lack of RAW format support for freescale V4L2 framework, I went ahead and applied the patch mentioned in https://community.freescale.com/thread/307065.
Now my configuration regsiters look better, though I am getting the same error. i have enabled more logging and below is the output. Any tip from the log?
In MVC: mxc_v4l_open
device name is Mxc Camera
End of mxc_v4l_open: v2f pix widthxheight 1280 x 720
End of mxc_v4l_open: crop_bounds widthxheight 1280 x 720
End of mxc_v4l_open: crop_defrect widthxheight 1280 x 720
End of mxc_v4l_open: crop_current widthxheight 1280 x 720
On Open: Input to ipu size is 1280 x 720
Pixel format is : IPU_PIX_FMT_GENERIC,0x32555049
Data written to CSI_SENS_CONF: 9b20
Sensor clock mode is: IPU_CSI_CLK_MODE_CCIR656_PROGRESSIVE
imx-ipuv3 imx-ipuv3.0: CSI_SENS_CONF = 0x00009B20
imx-ipuv3 imx-ipuv3.0: CSI_ACT_FRM_SIZE = 0x02CF04FF
mipi_reg during device init=330
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 80685600
case VIDIOC_QUERYCAP
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c02c563a
case VIDIOC_CROPCAP
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 4014563c
case VIDIOC_S_CROP
Cropping Input to ipu size 1280 x 720
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0cc5604
case VIDIOC_G_FMT
In MVC: mxc_v4l2_g_fmt type=1
type is V4L2_BUF_TYPE_VIDEO_CAPTURE
End of mxc_v4l2_g_fmt: v2f pix widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_bounds widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_defrect widthxheight 1280 x 720
End of mxc_v4l2_g_fmt: crop_current widthxheight 1280 x 720
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0145608
case VIDIOC_REQBUFS
In MVC:mxc_streamoff
MVC: In mxc_free_frame_buf
mxc_free_frame_buf: allocated buffer count = 0
In MVC:mxc_allocate_frame_buf - size=921600
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x18900, start=0x2aca3000, end=0x2ad84000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x18e00, start=0x2add6000, end=0x2aeb7000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x18f00, start=0x2aed5000, end=0x2afb6000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x19000, start=0x2b061000, end=0x2b142000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 40045612
case VIDIOC_STREAMON
In MVC:mxc_streamon with pixel format = 0x30314247
IPU:In csi_enc_enabling_tasks
In csi_enc_setup with format = 0x30314247, ipu = 0, csi = 0
cam->csi =0
setting up ipu csi enc with mipi vc = 0
imx-ipuv3 imx-ipuv3.0: init channel = 15
Inside _ipu_csi_init
Destination is CSI_DATA_DEST_IDMAC
setting up ipu 0 from csi_enc_setup with pixel format = 0x30555049
imx-ipuv3 imx-ipuv3.0: initializing idma ch 0 @ c08c0000
imx-ipuv3 imx-ipuv3.0: ch 0 word 0 - 00000000 00000000 00000000 E0002800 000B3C9F
imx-ipuv3 imx-ipuv3.0: ch 0 word 1 - 03220000 00644000 00C7C000 00013FC0 00000000
imx-ipuv3 imx-ipuv3.0: PFS 0x6,
imx-ipuv3 imx-ipuv3.0: BPP 0x5,
imx-ipuv3 imx-ipuv3.0: NPB 0x1f
imx-ipuv3 imx-ipuv3.0: FW 1279,
imx-ipuv3 imx-ipuv3.0: FH 719,
imx-ipuv3 imx-ipuv3.0: EBA0 0x19100000
imx-ipuv3 imx-ipuv3.0: EBA1 0x19100000
imx-ipuv3 imx-ipuv3.0: Stride 1279
imx-ipuv3 imx-ipuv3.0: scan_order 0
imx-ipuv3 imx-ipuv3.0: uv_stride 0
imx-ipuv3 imx-ipuv3.0: u_offset 0x0
imx-ipuv3 imx-ipuv3.0: v_offset 0x0
imx-ipuv3 imx-ipuv3.0: Width0 0+1,
imx-ipuv3 imx-ipuv3.0: Width1 0+1,
imx-ipuv3 imx-ipuv3.0: Width2 0+1,
imx-ipuv3 imx-ipuv3.0: Width3 0+1,
imx-ipuv3 imx-ipuv3.0: Offset0 0,
imx-ipuv3 imx-ipuv3.0: Offset1 0,
imx-ipuv3 imx-ipuv3.0: Offset2 0,
imx-ipuv3 imx-ipuv3.0: Offset3 0
In MVC:mxc_poll
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445611
case VIDIOC_DQBUF
In MVC:mxc_v4l_dqueue
In MVC:Dump Registers
In MVC:Inside Dump Registers
MIPI_CSI_N_LANES : 1
MIPI_CSI_PHY_SHUTDOWNZ : 1
MIPI_CSI_DPHY_RSTZ : 1
MIPI_CSI_CSI2_RESETN : 1
MIPI_CSI_PHY_STATE : 330
MIPI_CSI_DATA_IDS_1 : 0
MIPI_CSI_DATA_IDS_2 : 0
IPU1_CONF : 10000761
IPUx_INT_STAT_1 : 800000
IPUx_CSI0_DI : ffffff2b
IPU1_CSI0_SENS_CONF : 4009b20
IPU1_CSI0_SENS_FRM_SIZE : 2cf04ff
IPU1_CSI0_ACT_FRM_SIZE : 2cf04ff
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
In MVC:mxc_v4l_close
In MVC:mxc_streamoff
imx-ipuv3 imx-ipuv3.0: CSI stop timeout - 5 * 10ms
In MVC:mxc_free_frames
[520] : drivers/media/video/mxc/capture/imx219.c : ioctl_s_power() ENTER
[617] : drivers/media/video/mxc/capture/imx219.c : ioctl_s_power() EXIT
mxc_v4l_close: release resource
MVC: In mxc_free_frame_buf
mxc_free_frame_buf: allocated buffer count = -4
In MVC:mxc_free_frames
Dear Rejeesh Babu,
I'm new to this MIPI CSI interface and I have the custom camera, not able to get the a frame while running v4l2 application.
Can you please provide any suggestions on my issue ?
https://community.nxp.com/message/843732?commentID=843732#comment-843732
Much appreciated on your help.
I have solved the problem.
https://community.nxp.com/thread/437356
Hi All,
I managed to read few registers related to IPU and MIPI. One thing I quickly noticed is that, value of IPU1_CONF suggest that CSI0 if IPU1 is disabled (which is what I am trying to use!). Can somebdy let me know how to enable CSI0 if IPU1 (just writing to this bit from sensor driver is OK?).
Also, it would be great if someone could check the values of other registers as well and make more suggestions.
MIPI_CSI_N_LANES : 0x 1
MIPI_CSI_PHY_SHUTDOWNZ : 0x 1
MIPI_CSI_DPHY_RSTZ : 0x 1
MIPI_CSI_CSI2_RESETN : 0x 1
MIPI_CSI_PHY_STATE : 0x 630
MIPI_CSI_DATA_IDS_1 : 0x 0
MIPI_CSI_DATA_IDS_2 : 0x 0
IPU1_CONF : 0x660
IPUx_INT_STAT_1 : 0x800000
IPUx_CSI0_DI : 0xffffffff
IPU1_CSI0_SENS_CONF : 0x 0
IPU1_CSI0_SENS_FRM_SIZE : 0x 0
IPU1_CSI0_ACT_FRM_SIZE : 0x1df027f
Hi Rejeesh Babu,
In this file drivers/mxc/mipi/mxc_mipi_csi2.c
do the below change.
mipi_csi2_write(info, 0x00000014, MIPI_CSI2_PHY_TST_CTRL1);
mipi_csi2_write(info, 0x00000002, CSI2_PHY_TST_CTRL1); /* 110-125MHz */
Regards,
Aravinth
It did not help Aravind; btw how did you get this value? Also how do I ensure that my PIX_CLK (and any other clock related to capturing) is correct?
Hi Rejeesh,
From this ( Debug steps for customer MIPI sensor.docx ) freescale debug document they mentioned that PLL CLK(Differential clock)range.