Custom Location provider on AOSP kitkat 4.4.2 running on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom Location provider on AOSP kitkat 4.4.2 running on IMX6

566件の閲覧回数
kulbhushankashy
Contributor I

Hi All,

I am using IMX6's based custom board and It's running android AOSP version Kitkat 4.4.2. We have cellular module and wifi connectivity but don't have GPS on board. Now We want to develop one custom location provider which will use wifi and/or cellular module to get location. How I can develop it or is there any open source application available which can do this?

Regards,

-Kulbhushan

ラベル(5)
0 件の賞賛
1 返信

386件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kulbhushan

one can try to follow suggestions given on

http://stackoverflow.com/questions/18826718/how-to-get-location-with-wifi-in-android

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛