Hello community,
About VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,
It will dropped while wake from deep sleep mode.
(SABRE_SD_ILIMIT_disable_2P5_1P1_180518_224516_wakeup.png)
It seems that in-rush current to charge a bulk capacitor of NVCC_PLL_OUT.
So enabled current limit of LDO_1P1 by setting PMU_REG_1P1[ENABLE_ILIMIT] bit,
it seems that in-rush current is limited and voltage drop down has been resolved.
(SABRE_SD_ILIMIT_disable_2P5_enable_1P1_180518_225336_wakeup.png)
But lamp up of NVCC_PLL_OUT is slower than disable of current limit.
Is it OK to use a current limit function while wake up from deep sleep mode?
[Test environment]
Board : SABRE-SD i.MX6Q
OS : Linux BSP 4.9.11_1.0.0
Probe point :
ch1 : sh17 (VDDHIGH_IN)
ch2 : sh17 (VDDHIGH_IN)
ch3 : SW1_1 (CPUPWRON)
ch4 : R208 (NVCC_PLL_OUT)
Deep Sleep Mode :
Use a configuration of 5.2 Deep Sleep Mode (LPM6) in AN4509.
Best regards,
Ishii.
已解决! 转到解答。
Hi Ishii
>VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,
>It will dropped while wake from deep sleep mode
for VDDHIGH_IN voltage drop, may be useful to check comments on Sabre SD schematic
>Is it OK to use a current limit function while wake up from deep sleep mode?
yes, however additional time for slower ramp should be accounted in CCM_CLPCR
register STBY_COUNT settings, described in sect.18.6.18 CCM Low Power Control Register (CCM_CLPCR).
Procedure for exiting low power mode is described in sect.18.5.3.3.2 Exiting STOP
mode i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ishii
>VDDHIGH_IN voltage of SABRE_SD i.MX6Q board,
>It will dropped while wake from deep sleep mode
for VDDHIGH_IN voltage drop, may be useful to check comments on Sabre SD schematic
>Is it OK to use a current limit function while wake up from deep sleep mode?
yes, however additional time for slower ramp should be accounted in CCM_CLPCR
register STBY_COUNT settings, described in sect.18.6.18 CCM Low Power Control Register (CCM_CLPCR).
Procedure for exiting low power mode is described in sect.18.5.3.3.2 Exiting STOP
mode i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thank you for your quick response.
By attached waveform, a time of NVCC_PLL_OUT that voltage is ready are almost 440usec.
If it must wait more than 440usec as examples,
CKIL = 32.768KHz => 30.5usec period
440usec / 30.5usec = 14.42
to wait more than equal 15CKIL clock cycle so,
CCM_CGPR[PMIC_DELAY_SCALER] = 0 // clock is not divided
CCM_CLPCR[STBY_COUNT] = 11b // CCM will wait (15*pmic_delay_scaler)+1 ckil clock cycles = 16 CKIL clock cycle
or
CCM_CGPR[PMIC_DELAY_SCALER] = 1 // clock is divided /8
CCM_CLPCR[STBY_COUNT] = 01b // CCM will wait (3*pmic_delay_scaler)+1 ckil clock cycles = 25 CKIL clock cycle
Is it correct?
By the way, I found that NVCC_PLL_OUT and VDDHIGH_CAP are used 22uF for SABRE-SD board.
But these are requested to connect 10uF or small one in IMX6DQ6SDLHDG.
It seems a root cause of VDDHIGH_IN voltage drop down.
Is it OK to use 22uF capacitor?
Best regards,
Ishii.
Hi Ishii
provided my answer was just general recommendation.
i.MX6Q Sabre SD board works well with NXP BSPs described on
It is not recommended to change software and hardware configuration
for NVCC_PLL_OUT, as these are verified and work fine.
If customer wishes to proceed with own configuration suggest to use help
with Professional Services to have more detailed analysis and verification:
http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Best regards
igor
Hello Igor,
Thank you for your answer.
I understand your suggestion.
We will introduce my customer to use professional support if they need more verification
about their custom setting.
Best regards,
Ishii.