I download openwrt chaos calmer an using make menuconfig I create an image for imx233 but when I copy to SD card
The board load u-boot and the process end
I want a know how can I create an SD image with u-boot and openwrt starting files
Thanks for any advice on this issue
Sergio Sosa
Hi Sergio
nxp i.MX23 linux releases do not support openwrt, but one can check for example
https://wiki.openwrt.org/toh/olimex/imx233-olinuxino
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I download openwrt 15.05 branch (Chaos Calmer) using
git clone -b chaos_calmer git://github.com/openwrt/openwrt.git
run make menuconfig to configure it to target system "Freescale i.mx23/i.mx28" and target profile "Olimex Olinuxino maxi/mini boards"
run make V=s
and I obtain in the following dir ...bin/ mxs the next file
openwrt-mxs-olinuxino-maxi-sdcard-vfat-ext4.img
and using windows win32diskimager I copy to SD card
I load my custom board but my output is
The board uses a special boot image called bootstream / safeboot. The file includes a zImage, a compiled devicetree, and various preparation bootlets (power_, sdram_, linux_)- these are contained in package/imx-bootlets. The image is created by the elftosb tool.
My question is
How can i copy the correct files to SD card and with what tool
Thanks for your help
Sergio Sosa