Core performance difference between single core ad dual core on i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Core performance difference between single core ad dual core on i.MX6

729 次查看
norihiromichiga
Senior Contributor I

Hi,

I'm looking for benchmark test result which was captured on single core version of i.MX6 and dual core version of i.MX6, focusing on A9 core performance itself.

I can find some benchmark test results on i.MX6 Solo and dual cores(http://2014ftf.ccidnet.com/pdf/0058.pdf). But that benchmark is focusing on multimedia performance and hardware acceleration can affect the result.


I want to see benchmark test result using core intensive benchmark program on both dual core and single core.

Could someone advise me if I can find such benchmark test result on the internet?

Thanks,

Norihiro Michigami

0 项奖励
1 回复

416 次查看
igorpadykov
NXP Employee
NXP Employee

HI Norihiro

one can look at Coremark for Quad: 10370@4 cores, 10370/4 per core

EEMBC -- The Embedded Microprocessor Benchmark Consortium

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励