Core Frequency change of MIMX8ML6DVNLZAB(Consumer version) by temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Core Frequency change of MIMX8ML6DVNLZAB(Consumer version) by temperature

378件の閲覧回数
andy_kim
Contributor IV

Hello,

As far as I know,

The core frequency of iMX8M Plus is changed automatically by temperature from 1.8 GHz to 1.2 GHz.

Could you let me know the temperature range for each core frequency of 1.8GHz, 1.6GHz and 1.2GHz?

and Which document do I get the information with?

 

Thank you.

BR

Andy

0 件の賞賛
2 返答(返信)

375件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The thermal driver will monitor the SoC's temperature in a certain frequency to protect the SoC. It defines
three trip points: critical, hot, and active.
When reaching passive point, cooling device will lower CPU frequency and notify GPU/VPU to run at a lower frequency.
Details you can see the Thermal section in the i.MX_Reference_Manual.

0 件の賞賛

371件の閲覧回数
andy_kim
Contributor IV

Hello,

Thank you for your comment.

When I took a look at IMX8M Plus Reference Manual,  there are three temperature threshold register as below on it.

Immediate temperature threshold : TMHTITR

Average temperature threshold : TMHTATR

Average temperature threhold : TMHTACTR

 

However, there is no specific definition about the relation of core frequency change and the temperature threshold on IMX8M Plus Reference Manual.

Could you let me know where could I find the description between the temperature and core frequency as followings?

 

Core Frequency is 1.8GHz :  When Temperature range is under xx ℃  

Core Frequency is 1.6GHz : When Temperature range is between xx ℃  and xx ℃  

Core Frequency is 1.2GHz : When Temperature range is over xx ℃  

 

Best regards

Andy

0 件の賞賛