Hi,
I am trying to connect my BLE Client (iMXRT1060 +ublox module) with 2 servers (QN9090). I was able to successfully connect to one board and read the data. When I try to establish connection with both the servers only one gets connected and for the other module I get the error as below,
Found device:
Create connection failed (err -12)
I have configured the CONFIG_BT_MAX_CONN to 2 and have done the required modifications in the central_ht.c file to connect to 2 servers. But I understand from the above error that the SDK currently supports only one connection. Is that correct?
Is there any sample SDK to connect to multiple servers as we need to connect to multiple peripherals to get data. Your help on this is highly appreciated.
Thanks.
nxf56274 is my BLE colleague, he helps you test it today, please follow his code and test it on your side, whether it works or not?
Any updated information, please kindly let me know.
Best Regards,
Kerry
Hi,
Our requirement is to connect to multiple servers (atleast 3) to get the data. Since BLE can support a maximum of 7 connections at a time, should the sdk also support multiple connections? Can you help us with the changes to be done on the sdk side to support multiple connections?
Thanks.
Sorry, my previous reply is not correct, I checked with our BLE engineer, the client can connect more than 2 server at the same time.
Please refer to this application note at first:
https://www.nxp.com/docs/en/application-note/AN12414.pdf
If you still have question about it please kindly let me know.
Best Regards,
Kerry
Hi Kerry,
Does the edgefast bluetooth example in iMXRT 1060 SDK support multiple connections? I am using the ublox module so I have defined the macro WIFI_BOARD_AW_CM358. The sdk code for edgefast bluetooth is different from the freedom series code.
I have defined the macro CONFIG_BT_MAX_CONN to 2 and have also done changes in the central_ht.c file to support 2 connections. But looks like I can establish only one connection at a time.
In file bluetooth.h, what does the below macro mean?
/**
* @def BT_ID_DEFAULT
*
* Convenience macro for specifying the default identity. This helps
* make the code more readable, especially when only one identity is
* supported.
*/
#define BT_ID_DEFAULT 0
The above ID is used in bt_pal_conn.c etc. Does this mean the sdk currently supports only one connection?
Your help on this is highly appreciated.
Thanks.
Hi,
1 Comment the 'scan_start', Does it work with only one device?
2 If so, please try to create a thread. In the thread, the uart is waiting for the cmd to call the scan_start after the first device sending the data normally.
Hi,
Good morning. Now, I am trying to connect a third peripheral to my central device and I am able to establish a connection after connecting and subscribing to the first two peripherals. But after connecting the service discovery fails. The error code is 12 (ENOMEM). What does that mean?
Thanks.