I'm trying to connect an iphone over usb to an i.mx6d running Linux 3.14.52.
The initial configuration shows up correctly, but I don't get the following three alternate settings needed to handle the pairing and setting up usb tethering.
Is this a known issue?
I not getting any error messages from the ci_hdrc controller.
Any ideas that points me in the right direction is greatly appreciated.
Hi Robert
one can look at
USB dual role patch for Linux 3.10.17 BSP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your suggestion. The first patch was already applied. I applied the second, but I'm not getting any further.
It seems that I cannot set the controller into otg role instead of usb host. I don't get any input nodes in the sys/class directory mentioned and I'm missing the otg part of the debugfs.
Any further suggestions? Could it be that I miss something in the device-tree? Any example of a device-tree node where this works would be greatly appreciated.
/Robert
Further research suggests that dual role is only possible if using USB host0 on the imx6d, since that is the only one that supports OTG. The other three support host only. igorpadykov could you please confirm if this observation is correct? If that is the case I will need to request a hardware change in order to add iphone support to our system.
/Robert
Hi Robert
yes this is correct. For details please refer to Chapter 65
Universal Serial Bus Controller (USB) i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf
Best regards
igor