Hi viking_yuan
>Is it possible to set OTG2 as dual mode (OTG) and set OTG1 as host mode?
yes. For example one can look at sect.4.9.9 Changing the Controller Operation Mode
>If OTG1 is set as host mode, can we still use mfgtools to burn the images via the USB port of OTG1?
not. It should be in device mode for usage with mfgtools.
Best regards
igor
Hi igor,
According to https://community.nxp.com/t5/i-MX-Processors/Configure-USB-OTG2-port-in-peripheral-mode-in-iMX6-Eval... only one of the 2 OTGs can be configured as OTG mode. OTG1 has been configured as OTG mode because of the need to use mfgtools to burn images. So, it means that OTG2 would never be configured as OTG mode because OTG 1 has occupied the OTG setting. Is this correct?
Thanks!