hi, ALL
i encountered the following the problem when compile the QT(4.6) with LTIB
it's like libpng problem but i selected it in ltib.
What is missing or what is wrong?
Many thanks in advance
peter
-------------------------------------------------------------------------------------------------------------------------
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_get_valid'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_error_fn'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_create_info_struct'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_expand'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_read_info'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_write_info'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_strip_16'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_get_io_ptr'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_read_fn'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_write_image'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_destroy_read_struct'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_filler'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_IHDR'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_destroy_write_struct'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_oFFs'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_text'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_create_read_struct'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_sig_bytes'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_bgr'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_packing'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_get_IHDR'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_gAMA'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_compression_level'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_gray_to_rgb'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_tRNS'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_write_fn'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_get_x_pixels_per_meter'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_write_end'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_write_chunk'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_get_y_pixels_per_meter'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_read_end'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_set_packswap'
L3.0.35_4.1.0_130816_source/6Q/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/lib/libQtGui.so: undefined reference to `png_read_image'
已解决! 转到解答。