Hi All,
How can get compat drivers for wl12xx for kernel 3.14 version.
If any one used this kindly help me.
Thanks & Regards,
Lavanya
已解决! 转到解答。
Hi All ,
My wifi with wl12xx chip set is working fine with 3.14.28 kernel with dts file support compat-drivers are R8.6 version.
dts file settings
wlan_en_reg: fixedregulator {
compatible = "regulator-fixed";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-name = "wlan_enable_regulator";
gpio = <&gpio1 15 GPIO_ACTIVE_HIGH>; //active high
output-high;
enable-active-high;
};
pinctrl_usdhc1: usdhc1grp {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
MX6QDL_PAD_SD2_DAT1__GPIO1_IO14 0x13059
MX6QDL_PAD_SD2_DAT0__GPIO1_IO15 0x40013059
>;
};
&usdhc1 {
pinctrl-names = "default";
vmmc-supply = <&wlan_en_reg>;
bus-width = <4>;
pinctrl-0 = <&pinctrl_usdhc1>;
non-removable; /* non-removable is not a variable, the fact it is */
/* listed is all that is used by driver */
needs-special-hs-handling;
cap-power-off-card;
enable-sdio-wakeup;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@2 {
compatible = "ti,wl1271";
reg = <2>;
interrupt-parent = <&gpio1>;
interrupts = <14 IRQ_TYPE_LEVEL_HIGH>; /* gpio 14 */
ref-clock-frequency = <38400000>;
};
};
Thanks & Regards,
Lavanya
Hi All ,
My wifi with wl12xx chip set is working fine with 3.14.28 kernel with dts file support compat-drivers are R8.6 version.
dts file settings
wlan_en_reg: fixedregulator {
compatible = "regulator-fixed";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-name = "wlan_enable_regulator";
gpio = <&gpio1 15 GPIO_ACTIVE_HIGH>; //active high
output-high;
enable-active-high;
};
pinctrl_usdhc1: usdhc1grp {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
MX6QDL_PAD_SD2_DAT1__GPIO1_IO14 0x13059
MX6QDL_PAD_SD2_DAT0__GPIO1_IO15 0x40013059
>;
};
&usdhc1 {
pinctrl-names = "default";
vmmc-supply = <&wlan_en_reg>;
bus-width = <4>;
pinctrl-0 = <&pinctrl_usdhc1>;
non-removable; /* non-removable is not a variable, the fact it is */
/* listed is all that is used by driver */
needs-special-hs-handling;
cap-power-off-card;
enable-sdio-wakeup;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@2 {
compatible = "ti,wl1271";
reg = <2>;
interrupt-parent = <&gpio1>;
interrupts = <14 IRQ_TYPE_LEVEL_HIGH>; /* gpio 14 */
ref-clock-frequency = <38400000>;
};
};
Thanks & Regards,
Lavanya
Hi Lavanya
please look at
en/users/Drivers/wl12xx - Linux Wireless
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi All,
I am using R8.6 wifi compat drivers,
I can able to load the drivers
compat.ko,
cfg80211.ko
mac80211ko
wlcore.ko
wlcore_sdio.ko
wl12xx.ko
wl18xx.ko
But i am not getting wlan0 node in ifconfig -a
ifconfig wlan0 up is giving error no such file