Chromium in i.MX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chromium in i.MX8M Mini

1,266 Views
deeksha
Contributor III

Hello ,

I am working on i.MX8 M Mini L5.4.70. 

-> I have to run graphical application in Chromium[Chromium 83.0.4103.116 stable] web browser. When i tried to binary i got below output.

./chromium 

[3448:3448:0704/135507.957736:ERROR:zygote_host_impl_linux.cc(89)] Running as root without --no-sandbox is not supported. See https://crbug.com/638180.

So i tried by running ./chromium --no-sandbox 

chromium application started running. I was getting few more prints on terminal.

[3456:3522:0704/135940.678458:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.DBus.Properties.Get: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: The s
[3456:3522:0704/135940.679404:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.UPower.GetDisplayDevice: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: s
[3456:3522:0704/135940.680265:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.UPower.EnumerateDevices: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: s

[ 4375.730017] alloc_contig_range: [61a00, 61dc0) PFNs busy
[ 4380.382574] alloc_contig_range: [61200, 615c0) PFNs busy
[ 4384.598200] alloc_contig_range: [61a00, 61dc0) PFNs busy

[2494:2519:0701/131603.017528:ERROR:batching_media_log.cc(38)] MediaEvent: {"error":"FFmpegDemuxer: no supported streams"}
[2494:2494:0701/131603.038328:ERROR:batching_media_log.cc(35)] MediaEvent: {"pipeline_error":14}
[2494:2494:0701/131603.039073:ERROR:batching_media_log.cc(35)] MediaEvent: {"pipeline_error":14}

when i tried to run application in chromium , it started using more of CPU. so i tried to enable hardware acceleration to enable GPU but I noticed either chromium hangs or crashes with segmentation fault if tried to press setting or tab.

I checked gpu details in chromium , 

Graphics Feature Status
Canvas: Hardware accelerated
Flash: Hardware accelerated
Flash Stage3D: Hardware accelerated
Flash Stage3D Baseline profile: Hardware accelerated
Compositing: Hardware acceleration 
Multiple Raster Threads: Enabled
Out-of-process Rasterization: Disabled
OpenGL: Enabled
Hardware Protected Video Decode: Unavailable
Rasterization: Software only. Hardware acceleration disabled
Skia Renderer: Enabled
Video Decode: Unavailable
Vulkan: Disabled
WebGL: Hardware accelerated
WebGL2: Hardware accelerated 

I disabled hardware acceleration and i noticed  gpu details attached in chromium_gpu.txt file.

May I know why I am facing above issues. Any solutions for this

Thanks and Regards,

Deeksha

 

Labels (1)
0 Kudos
2 Replies

1,258 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello deeksha,

 

Chromium run without GPU, that a current issue, you may try the 5.15 BSP

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Regards

1,211 Views
deeksha
Contributor III

Hi,

whether 5.15 BSP [91.0.4472.114] has solution for my issue ?

Is it possible to update 5.4.70 BSP with Chromium version 91.0.4472.114 ?

 

Regards,

Deeksha

0 Kudos