Hello ,
I am working on i.MX8 M Mini L5.4.70.
-> I have to run graphical application in Chromium[Chromium 83.0.4103.116 stable] web browser. When i tried to binary i got below output.
./chromium
[3448:3448:0704/135507.957736:ERROR:zygote_host_impl_linux.cc(89)] Running as root without --no-sandbox is not supported. See https://crbug.com/638180.
So i tried by running ./chromium --no-sandbox
chromium application started running. I was getting few more prints on terminal.
[3456:3522:0704/135940.678458:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.DBus.Properties.Get: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: The s
[3456:3522:0704/135940.679404:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.UPower.GetDisplayDevice: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: s
[3456:3522:0704/135940.680265:ERROR:object_proxy.cc(632)] Failed to call method: org.freedesktop.UPower.EnumerateDevices: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: s
[ 4375.730017] alloc_contig_range: [61a00, 61dc0) PFNs busy
[ 4380.382574] alloc_contig_range: [61200, 615c0) PFNs busy
[ 4384.598200] alloc_contig_range: [61a00, 61dc0) PFNs busy
[2494:2519:0701/131603.017528:ERROR:batching_media_log.cc(38)] MediaEvent: {"error":"FFmpegDemuxer: no supported streams"}
[2494:2494:0701/131603.038328:ERROR:batching_media_log.cc(35)] MediaEvent: {"pipeline_error":14}
[2494:2494:0701/131603.039073:ERROR:batching_media_log.cc(35)] MediaEvent: {"pipeline_error":14}
when i tried to run application in chromium , it started using more of CPU. so i tried to enable hardware acceleration to enable GPU but I noticed either chromium hangs or crashes with segmentation fault if tried to press setting or tab.
I checked gpu details in chromium ,
Graphics Feature Status
Canvas: Hardware accelerated
Flash: Hardware accelerated
Flash Stage3D: Hardware accelerated
Flash Stage3D Baseline profile: Hardware accelerated
Compositing: Hardware acceleration
Multiple Raster Threads: Enabled
Out-of-process Rasterization: Disabled
OpenGL: Enabled
Hardware Protected Video Decode: Unavailable
Rasterization: Software only. Hardware acceleration disabled
Skia Renderer: Enabled
Video Decode: Unavailable
Vulkan: Disabled
WebGL: Hardware accelerated
WebGL2: Hardware accelerated
I disabled hardware acceleration and i noticed gpu details attached in chromium_gpu.txt file.
May I know why I am facing above issues. Any solutions for this
Thanks and Regards,
Deeksha
Hello deeksha,
Chromium run without GPU, that a current issue, you may try the 5.15 BSP
Regards