Hello Team,
I want to build Camera based application in custom i.MX8M Nano based Processor.
So for that I need to build Yocto Project Image for our custom board.
So can you suggest the appropriate image option for the same?
I use "fsl-imx-wayland" as a Distro and "imx8mnevk" as a Machine.
Would i select "core-image-base or else other one?
Or is there any sample application available in any image for camera related?
can you help me out?
Thank You
已解决! 转到解答。
refer to the user guide:
core-image-base:A console-only image that fully supports the target device
hardware.
it seems that this image doesn't includes the camera application, shouldn't include multimedia application, but I never tested this image, I suggest that you can use imx-image-multimedia, we all use this image and imx-image-full
first, you can refer to the yocto user guide, if you use 8mn, you can choose the machine name
for example,
$ DISTRO=fsl-imx-xwayland MACHINE=imx8mnevk source imx-setup-release.sh -b build-xwayland
$ bitbake imx-image-full
these commands are full image based on xwayland backend, you can change image what you need, pls refer to the Table 1. i.MX Yocto project images of yocto user guide, you also can change fsl-imx-xwayland fsl-imx-wayland
refer to the user guide:
core-image-base:A console-only image that fully supports the target device
hardware.
it seems that this image doesn't includes the camera application, shouldn't include multimedia application, but I never tested this image, I suggest that you can use imx-image-multimedia, we all use this image and imx-image-full