Hello all.
I am new to building bootloader by using SDK. I managed to create a "u-boot.imx" file. However, I want to add custom text to console during boot sequence. I do not know which file to modify. Could you help me with this problem?
________________________________________________________________________
For example:
U-Boot 2015.04+fslc+g5d9ffd2 (Oct 03 2017 - 12:30:19)
<CUSTOM TEXT>
CPU: Freescale i.MX6Q rev1.5 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 21C
Reset cause: POR
Board: Come-imx6q-100
I2C: ready
DRAM: 2 GiB
<CUSTOM TEXT> ... continues
_________________________________________________________________________
Many thanks.
已解决! 转到解答。
Hi Giray
please look at attached Porting Guide Chapter 3 Porting U-Boot
mentioned text can be changed in uboot/arch/arm/imx-common/cpu.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Giray
please look at attached Porting Guide Chapter 3 Porting U-Boot
mentioned text can be changed in uboot/arch/arm/imx-common/cpu.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------