Hi Everyone
insmod ov5640_mipi.c module is loaded and it showing mipi is found but when we are trying to insert mxc_v4l2_capture.ko it showin ERROR: v4l2 capture: slave not found!
when i am trying this command
gst-launch-1.0 imxv4l2src num-buffers=300 device="$CAM-DEV" ! imxv4l2sink device=/dev/video17
Can't get caps from capture device, use the default setting.
Perhaps haven't capture device.
====== IMXV4L2SRC: 4.0.3 build on Aug 2 2016 18:40:00. ======
set color key:00010203
====== IMXV4L2SINK: 4.0.3 build on Aug 2 2016 18:40:01. ======
Setting pipeline to PAUSED ...
display(/dev/fb0) resolution is (800x480).
ERROR: Pipeline doesn't want to pause.
Setting pipeline to NULL ...
Freeing pipeline ...
Thankyou
已解决! 转到解答。
Hi sindhuja,
It looks like there is no image data on /dev/video17, check if your ov5640 is running correctly, check the driver info:
# v4l2-ctl -d /dev/video17 --all
previous thread should be helpful:
OV5640 mipi camera on mcimx6q-sdb
gstreamer and ov5640 mipi camera
regards
Hi sindhuja,
It looks like there is no image data on /dev/video17, check if your ov5640 is running correctly, check the driver info:
# v4l2-ctl -d /dev/video17 --all
previous thread should be helpful:
OV5640 mipi camera on mcimx6q-sdb
gstreamer and ov5640 mipi camera
regards
Hi,
Thanks for the reply by this command i am getting this information
# v4l2-ctl -d /dev/video17 --all1cf351/kernel/drivers/media/plat
Driver Info (not using libv4l2):
Driver name : mxc_vout
Card type : DISP3 FG
Bus info :
Driver version: 3.14.28
Capabilities : 0x04000002
Video Output
Streaming
Format Video Output:
Width/Height : 320/240
Pixel Format : ''
Field : Any
Bytes per Line: 0
Size Image : 76800
Colorspace : Unknown (00000000)
Crop Capability Video Output:
Bounds : Left 0, Top 0, Width 800, Height 480
Default : Left 0, Top 0, Width 800, Height 480
Pixel Aspect: 0/0
horizontal_flip (bool) : default=0 value=0
vertical_flip (bool) : default=0 value=0
rotate (int) : min=0 max=270 step=90 default=0 value=0
This is what my device is showing i am not understanding device is working or not please help thanks in advance
Thankyou