Cannot find imx_3.10.17_1.0.2_ga on freescale git....

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot find imx_3.10.17_1.0.2_ga on freescale git....

1,589 Views
Selea
Senior Contributor I

I read that it was released a new ga patch release imx_3.10.17_1.0.2_ga

but i cannot find the banch on linux-2.6-imx.git - Freescale i.MX Linux Tree

anyone can explain it to me?

I'm downloading this from freescale IMX6Q page:

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.2_iMX6QDLS_BUNDLE&appType=license&loc...

but should not it be just binary and DOC...

"

L3.10.17_1.0.2_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation.

Size (K): 717480 Format: gz Rev #: L3.10.17_1.0.2 Modified: 10/29/2014

"

Let me understand please.

I expect to find a new branch on the git...


Thanks

Omar



Tags (1)
5 Replies

961 Views
Yuri
NXP Employee
NXP Employee

Please use the Release notes :

http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf

Summary page :

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

961 Views
LuisCasado
NXP Employee
NXP Employee

Hi Omar,

You have to use :

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.2_ga

The kernel branch is the same.

Regards,

Luis

0 Kudos

960 Views
Selea
Senior Contributor I

do you mean that the kernel branch is the same and the patch is on other packets in the distribution builde with yocto?

Omar

0 Kudos

960 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

The Yocto recipe for kernel in release 1.0.2 says:

SRC_URI = "git://${FSL_ARM_GIT_SERVER}/linux-2.6-imx.git;protocol=git;branch=imx_3.10.17_1.0.0_ga"

Regards,

Luis

0 Kudos

960 Views
Selea
Senior Contributor I

i'm working on the kernel manually out of yocto frame...

so i should make

git checkout -b imx-3.10.17-1.0.2_ga

but if you look at the http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/refs/heads?h=imx_3.10.17_1.0.1_ga

the branch 1.0.2_ga is not there?

so i'm missing something....

in the archive downloaded from the www.freescale.com i have infact just binary and doc.... but where is the source ?

Thanks

Omar

0 Kudos