Can we use 64MB NOR Flash with iMX6solo GPMI interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can we use 64MB NOR Flash with iMX6solo GPMI interface?

802 次查看
deepaktajanpure
Contributor II

I want to use iMx6Solo. I have gone through i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 5, 05/2020 Page 209. Document is saying Feature that : Nand-Flash (MLC up to 40-bit ECC) and NOR Flash memory interface via GPMI Nand-Flash controller.

 

But After going through GPMI chapter in detail I didn't found NOR Flash.

So my question is "Can we use 64MB NOR Flash with iMX6solo GPMI interface?"

0 项奖励
回复
4 回复数

769 次查看
deepaktajanpure
Contributor II

If we want to use SPI NOR Flash as Boot Flash then what will be max size SPI NOR Flash in iMx6Solo?

0 项奖励
回复

779 次查看
jimmychan
NXP TechSupport
NXP TechSupport

GPMI is for NAND flash only.

0 项奖励
回复

765 次查看
deepaktajanpure
Contributor II
If we want to use SPI NOR Flash as Boot Flash then what will be max size SPI NOR Flash in iMx6Solo?
0 项奖励
回复

753 次查看
jimmychan
NXP TechSupport
NXP TechSupport

According to the boot_cfg4, the ecspi address is 1-3 bytes. 3 bytes mean 16MB.

0 项奖励
回复